spi receive data via dma
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-12-02 9:15 AM
Posted on December 02, 2013 at 18:15
i traied to recive data from another stm32f4 via SPI that's why i used the dma to receive data from SPI
GPIO_InitTypeDef GPIO_InitStructure;uint16_t value;void init_SPI(void) { GPIO_InitTypeDef GPIO_InitStruct; SPI_InitTypeDef SPI_InitStruct; DMA_InitTypeDef DMA_InitStructure; // enable clock for used IO pins RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); /* DMA2 Stream0 channel0 configuration **************************************/DMA_InitStructure.DMA_Channel = DMA_Channel_0;DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)Buffer;DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)(SPI1->DR); DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte;DMA_InitStructure.DMA_PeripheralDataSize = DMA_MemoryDataSize_Byte;DMA_InitStructure.DMA_DIR = DMA_DIR_MemoryToPeripheral;DMA_InitStructure.DMA_Mode = DMA_Mode_Normal;DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;DMA_InitStructure.DMA_BufferSize = 6*84;DMA_InitStructure.DMA_Priority = DMA_Priority_High;DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable; DMA_Init(DMA1_Stream4, &DMA_InitStructure);DMA_Cmd(DMA1_Stream4, ENABLE); // ...SPI_I2S_DMACmd(SPI1, SPI_I2S_DMAReq_Tx, ENABLE); /* configure pins used by SPI1 * PA5 = SCK * PA6 = MISO * PA7 = MOSI */ GPIO_InitStruct.GPIO_Pin = GPIO_Pin_7 | GPIO_Pin_6 | GPIO_Pin_5; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStruct.GPIO_OType = GPIO_OType_PP; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStruct); // connect SPI1 pins to SPI alternate function GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_SPI1); GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_SPI1); GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_SPI1); GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_AF_SPI1); // enable clock for used IO pins /* Configure the chip select pin in this case we will use PA4 */ GPIO_InitStruct.GPIO_Pin = GPIO_Pin_4; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStruct.GPIO_OType = GPIO_OType_PP; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOA, &GPIO_InitStruct); // enable peripheral clock RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE); /* configure SPI1 in Mode 0 * CPOL = 0 --> clock is low when idle * CPHA = 0 --> data is sampled at the first edge */ SPI_InitStruct.SPI_Direction = SPI_Direction_2Lines_FullDuplex; // set to full duplex mode, seperate MOSI and MISO lines SPI_InitStruct.SPI_Mode = SPI_Mode_Slave; // transmit in master mode, NSS pin has to be always high SPI_InitStruct.SPI_DataSize = SPI_DataSize_8b; // one packet of data is 8 bits wide SPI_InitStruct.SPI_CPOL = SPI_CPOL_Low; // clock is low when idle SPI_InitStruct.SPI_CPHA = SPI_CPHA_1Edge; // data sampled at first edge SPI_InitStruct.SPI_NSS = SPI_NSS_Soft | SPI_NSSInternalSoft_Set; // set the NSS management to internal and pull internal NSS high SPI_InitStruct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_4; // SPI frequency is APB2 frequency / 4 SPI_InitStruct.SPI_FirstBit = SPI_FirstBit_MSB;// data is transmitted MSB first SPI_Init(SPI1, &SPI_InitStruct); SPI_Cmd(SPI1, ENABLE); // enable SPI1}int main(void){ init_SPI(); STM32F4_Discovery_LEDInit(LED3); STM32F4_Discovery_LEDInit(LED4); STM32F4_Discovery_LEDInit(LED5); STM32F4_Discovery_LEDInit(LED6); while(1) { value=SPI_I2S_ReceiveData(SPI1);if (value<400)STM32F4_Discovery_LEDOn(LED5), STM32F4_Discovery_LEDOff(LED6);else if (value >400) STM32F4_Discovery_LEDOn(LED6),STM32F4_Discovery_LEDOff(LED5);;} }
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-12-02 9:43 AM
Posted on December 02, 2013 at 18:43
I'm confused, DMA RX on SPI1 in Slave Mode?
Look to be using the wrong DMA, Channel and Stream for that. Not enabling DMAx unit clock. Data direction of DMA is wrong. The code seems to be a random mix of cut-n-paste with no cohesive plan. SPI1 would use DMA2, Channel 3, Stream 0 or 2 for reception of data, to send data (from a slave to master) you'd transmit via DMA2, Channel 3, Stream 3 or 5
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-12-03 1:13 AM
Posted on December 03, 2013 at 10:13
DMA_InitStructure.DMA_DIR = DMA_DIR_
Peripheral
ToMemory;DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)(&(SPI1->DR));