2013-04-30 1:51 AM
Hello,
I have a problem with SPI communication in case of NSS Hardware control. NSS of SPI Signal is always low. I know that it is low when SPI is enable, and high when SPI is disable. But it is always low. why? The following is my program related with SPI. ============================================================== void bsp_init_rcc(void) { /* SYSCLK, HCLK, PCLK2 and PCLK1 configuration -----------------------------*/ /* RCC system reset(for debug purpose) */ RCC_DeInit();/* Enable HSE */
RCC_HSEConfig(RCC_HSE_ON);/* Wait till HSE is ready */
HSEStartUpStatus = RCC_WaitForHSEStartUp();if (HSEStartUpStatus == SUCCESS)
{ /* Enable Prefetch Buffer */ FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable);/* Flash 2 wait state */
FLASH_SetLatency(FLASH_Latency_2);/* HCLK = SYSCLK */
RCC_HCLKConfig(RCC_SYSCLK_Div1);/* PCLK2 = HCLK */
RCC_PCLK2Config(RCC_HCLK_Div1); /* PCLK2 = HCLK/2 */ // RCC_PCLK2Config(RCC_HCLK_Div2);/* PCLK1 = HCLK/2 */
RCC_PCLK1Config(RCC_HCLK_Div2);#if defined( STM32F10X_CL )
/* Configure PLLs *********************************************************/ /* PLL2 configuration: PLL2CLK = (HSE / 5) * 8 = 40 MHz */ RCC_PREDIV2Config(RCC_PREDIV2_Div5); RCC_PLL2Config(RCC_PLL2Mul_8);/* Enable PLL2 */
RCC_PLL2Cmd(ENABLE);/* Wait till PLL2 is ready */
while (RCC_GetFlagStatus(RCC_FLAG_PLL2RDY) == RESET) {}#if defined (HSE_8MHZ)
/* PLL configuration: PLLCLK = (PLL2 / 5) * 9 = 72 MHz */ RCC_PREDIV1Config(RCC_PREDIV1_Source_PLL2, RCC_PREDIV1_Div5); RCC_PLLConfig(RCC_PLLSource_PREDIV1, RCC_PLLMul_9); #endif #else#if defined (HSE_12MHZ)
/* PLLCLK = 12MHz * 6 = 72 MHz */ RCC_PLLConfig(RCC_PLLSource_HSE_Div1, RCC_PLLMul_6); #elif defined( HSE_16MHZ ) /* PLLCLK = 16MHz /2 * 9 = 72 MHz */ RCC_PLLConfig(RCC_PLLSource_HSE_Div2, RCC_PLLMul_9); #else // 8MHZ /* PLLCLK = 8MHz * 9 = 72 MHz */ RCC_PLLConfig(RCC_PLLSource_HSE_Div1, RCC_PLLMul_9); #endif #endif/* Enable PLL */
RCC_PLLCmd(ENABLE);/* Wait till PLL is ready */
while (RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET) { }/* Select PLL as system clock source */
RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);/* Wait till PLL is used as system clock source */
while(RCC_GetSYSCLKSource() != 0x08) { } } else { /* If HSE fails to start-up, the application will have wrong clock configuration. User can add here some code to deal with this error *//* Go to infinite loop */
while (1) { } } /* enable the PWR clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE);/* Enable GPIOA, GPIOB, GPIOC, GPIOD, GPIOE and AFIO clocks */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB |RCC_APB2Periph_GPIOC | RCC_APB2Periph_GPIOD | RCC_APB2Periph_GPIOE | RCC_APB2Periph_AFIO, ENABLE);/* USART1 Periph clock enable */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);/* TIM1 Periph clock enable */
// RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE);/* TIM2 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);Set_USBClock();
/* Enable peripheral clocks --------------------------------------------------*/
/* SPI1 clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);/* SPI2 Periph clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE); }void bsp_init_gpio(void)
{ GPIO_InitTypeDef GPIO_InitStructure;/* Configure the GPIO ports( leds ) */
GPIO_InitStructure.GPIO_Pin = LED_USER_PIN; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(LED_USER_PORT, &GPIO_InitStructure);/* GPIOA Configuration:TIM2 Channel1, 2, 3 and 4 in Output */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure);/* Configure SPI1 pins: SCK, MISO and MOSI ---------------------------------*/
/* Confugure NSS, SCK and MOSI pins as Alternate Function Push Pull */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_7; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Confugure MISO pin as Input Floating */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &GPIO_InitStructure); }void spi_test(void)
{ /* SPI1 configuration ------------------------------------------------------*/ SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low; SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Hard; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_4; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_Init(SPI1, &SPI_InitStructure); /* Enable SPI1 CRC calculation */ SPI_CalculateCRC(SPI1, ENABLE);SPI_SSOutputCmd(SPI1, ENABLE);
/* Enable SPI1 */
SPI_Cmd(SPI1, ENABLE);/* Transfer procedure */
/* Wait for SPI1 Tx buffer empty */ while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET);/* Send SPI2 data */
SPI_I2S_SendData(SPI1, SPI1_Buffer_Tx[TxIdx++]); } ============================================================== Is there any error for NSS Control?2013-04-30 2:05 PM