2025-07-02 9:12 AM - edited 2025-11-23 9:34 AM
Hi,
I am using an STM32H7RSxx device and I need to use the SPI6 (both full and half duplex) with the DMA.
The problem I am facing on is the MOSI pin doesn't transmit anything.Only the SCK is working.
Despite having configured it for SPI6 Alternate Function (according to datasheet)
// SPI6 pins
// SCLK, MISO, MISO, NSS
GPIO_InitStruct.Pin = LL_GPIO_PIN_4 | LL_GPIO_PIN_5 | LL_GPIO_PIN_6 | LL_GPIO_PIN_7;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_UP;
GPIO_InitStruct.Alternate = LL_GPIO_AF_8;
LL_GPIO_Init(GPIOA, &GPIO_InitStruct);it always stays to low level.
What is strange is the fact that if I use PB5 as SPI6 MOSI
I can see as the pin stays at high level in idle state, but low for the rest of transmission, and this is quiet confusing.
If I am not blind at all, the TRM and datasheet does not say anything about it..
Of course the DMA transmission buffer is not zero.
I have read on another post that the order of initialization can matter, but honestly, I could not figure out the solution.
I attached a small working example of what I am doing, I hope I will receive some hint.
Thanks,
s.
Solved! Go to Solution.
2025-07-05 6:56 AM - edited 2025-07-05 6:57 AM
Does MOSI transmit something non-zero if you use a blocking SPI call? HAL_SPI_TransmitReceive?
> SCB_InvalidateDCache_by_Addr(&dmaTxBuff, DMA_TXRX_BUFF_SIZE);
> SpiDmaTrf((uint32_t) &dmaTxBuff, (uint32_t) &dmaRxBuff);
If data cache is disabled, why are you calling invalidate here? If it was enabled, you should be calling clean, not invalidate.
Your buffers aren't aligned to a cache page, so using cache is not an option here.
Still think this is a cache issue.
2025-07-05 7:33 AM - edited 2025-07-05 7:47 AM
2025-07-09 1:28 AM - edited 2025-07-09 2:33 AM
I finally think I found the final solution to this issue, which seems to be related also with the port allocation of the DMA: concretely, choosing the PORT #1 (#0 doesn't work) as follows:
LL_DMA_SetLinkAllocatedPort(p_dma, p_channel, LL_DMA_LINK_ALLOCATED_PORT1);
LL_DMA_SetSrcAllocatedPort(p_dma, p_channel, LL_DMA_LINK_ALLOCATED_PORT1);
LL_DMA_SetDestAllocatedPort(p_dma, p_channel, LL_DMA_LINK_ALLOCATED_PORT1);Thanks @TDK for your time, your suggestions about cache handling have been very useful.
s.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.