Skip to main content
Associate II
May 5, 2024
Question

SPI for LCD failed to transmit data on STM32F103VET6

I'm trying to initialize an LCD module (ST7796U controller) on a STM32F103VET6 development board using SPI1, yet the souce code I got from the seller is using software-simulated SPI instead of hardware SPI (with SPI1_NSS enabled as output):

 

 

 

#define LCD_SCLK_Clr() HAL_GPIO_WritePin(GPIOA,GPIO_PIN_5,GPIO_PIN_RESET) 

#define LCD_SCLK_Set() HAL_GPIO_WritePin(GPIOA,GPIO_PIN_5,GPIO_PIN_SET) 

#define LCD_MOSI_Clr() HAL_GPIO_WritePin(GPIOA,GPIO_PIN_7,GPIO_PIN_RESET) 

#define LCD_MOSI_Set() HAL_GPIO_WritePin(GPIOA,GPIO_PIN_7,GPIO_PIN_SET)

//the above are located in lcd_init.h, which I cannot attach due to the attachments number limit

void LCD_Write_Bus(uint8_t dat){

 uint8_t i; 

 for(i=0;i<8;i++) { 

 LCD_SCLK_Clr(); 

 if(dat&0x80) { LCD_MOSI_Set();

 } 

 else { LCD_MOSI_Clr(); 

 } 

 LCD_SCLK_Set(); 

 dat<<=1; }
}

 

 

and the following is my work:

 

void LCD_Write_Bus(uint8_t dat){
 HAL_SPI_Transmit_DMA(&hspi1, &dat, 1);
 while (HAL_SPI_GetState(&hspi1) != HAL_SPI_STATE_READY){
 __NOP;
 }
}

 

but the LCD module does not show up anything after i initialize the LCD and call the FillColor function in main.c, only the backlight is enabled.

 

is there any problem with my code?

 

the edited lcd.c and lcd_init.c is attached, if there is any strange chinese characters, don't worry, they are comments, just ignored them.

 

thanks!

This topic has been closed for replies.

2 replies

AScha.3
Super User
May 5, 2024

>LCD module does not show up anything after i initialize the LCD

So : no working init.

>is there any problem with my code?

A: LCD wrong connected

B: spi timing/signals wrong

C: LCD init sequence wrong  (one wrong byte is enough ! )

D : your program .... (with DMA i had not much luck on my TFTs , cpu/dma to fast for the TFT chip.)

You can choose now .... :)

 

Or begin with A , check it 100% ; then B... (need ds of display, to check timing in specs ); then...

If you feel a post has answered your question, please click on " Best Answer ".
Andrew Neil
Super User
May 10, 2024

@OW1TY2 wrote:

SPI for LCD failed to transmit data on STM32F103VET6


How do you know that it's failed to transmit?

As @AScha.3 said, use an oscilloscope to verify that the SPI lines are actually behaving as required...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.