2025-06-11 8:36 AM
Hey, I'm just trying to use the BLE STM32UB5x in the board B-U585I-IOT02A. I used the following configurations for the STM32CubeProgrammer like suggested here (https://wiki.st.com/stm32mcu/wiki/Connectivity:STM32WB_BLE_Hardware_Setup)
Then, I switch SW4 ON, SW5 OFF and added this to main.c
/* USER CODE BEGIN 0 */
static HAL_StatusTypeDef BLE_SendCmd(const char *cmd) {
HAL_StatusTypeDef ret;
const char crlf[] = "\r\n";
char response[64] = {0};
printf("Sending BLE command: %s\r\n", cmd);
ret = HAL_UART_Transmit(&huart4, (uint8_t *)cmd, strlen(cmd), 100);
ret |= HAL_UART_Transmit(&huart4, (uint8_t *)crlf, sizeof(crlf)-1, 100);
if (ret != HAL_OK) {
printf("UART transmit failed (err: %d)\r\n", ret);
return ret;
}
HAL_Delay(50);
ret = HAL_UART_Receive(&huart4, (uint8_t *)response, sizeof(response)-1, 100);
if (ret == HAL_OK) {
printf("BLE response: %s\r\n", response);
} else {
printf("No response or receive error (err: %d)\r\n", ret);
}
return ret;
}
static void BLE_StartAdvertising(void) {
if (BLE_SendCmd("AT") != HAL_OK) {
printf("BLE check failed. BLE modue may not be responsive.\r\n");
return;
}
if (BLE_SendCmd("AT+BLEADVSTART") != HAL_OK) {
printf("Failed to start BLE advertising.\r\n");
return;
}
printf("BLE advertising started successfully.\r\n");
}
/* USER CODE END 0 *//* USER CODE BEGIN 2 */
BLE_StartAdvertising();
/* USER CODE END 2 */
And in the terminal I get this:
Sending BLE command: AT
No response or receive error (err: 3)
BLE check failed. BLE modue may not be responsive.
Any help would be appreciated, thank you!