SPI Communication between 2 - STM32 Discovery Board
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-05-07 10:04 AM
Posted on May 07, 2015 at 19:04
I am novice to ST family.
I have written code for SPI communication between Master and Slave . But I am unable to identify errors.Master Device Program
&sharpinclude ''stm32f4xx.h'' void SPIInit(void); __IO uint8_t received_val = 0; int main(void) { SPIInit(); while(1) { GPIO_ResetBits(GPIOE,GPIO_Pin_7); while(!SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_TXE)); SPI_I2S_SendData(SPI2, 0x9C); Delay(0x3FFFFF); while(!SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_RXNE)); received_val = SPI_I2S_ReceiveData(SPI2); GPIO_SetBits(GPIOE,GPIO_Pin_7); } } void SPIInit(void){ GPIO_InitTypeDef GPIO_InitStruct; SPI_InitTypeDef SPI_InitStruct; RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB | RCC_AHB1Periph_GPIOE , ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15 ; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStruct.GPIO_OType = GPIO_OType_PP; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOB, &GPIO_InitStruct); GPIO_PinAFConfig(GPIOB, GPIO_PinSource13, GPIO_AF_SPI2); GPIO_PinAFConfig(GPIOB, GPIO_PinSource14, GPIO_AF_SPI2); GPIO_PinAFConfig(GPIOB, GPIO_PinSource15, GPIO_AF_SPI2); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_7 ; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStruct.GPIO_OType = GPIO_OType_PP; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOE, &GPIO_InitStruct); SPI_InitStruct.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStruct.SPI_Mode = SPI_Mode_Master; SPI_InitStruct.SPI_DataSize = SPI_DataSize_8b; SPI_InitStruct.SPI_CPOL = SPI_CPOL_Low; SPI_InitStruct.SPI_CPHA = SPI_CPHA_1Edge; SPI_InitStruct.SPI_NSS = SPI_NSS_Hard; SPI_InitStruct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_256; SPI_InitStruct.SPI_FirstBit = SPI_FirstBit_MSB; SPI_Init(SPI2, &SPI_InitStruct); SPI_SSOutputCmd(SPI2, ENABLE); SPI_Cmd(SPI2, ENABLE); }Slave Device Code
&sharpinclude ''stm32f4xx.h'' void SPIInit(void); void Delay(__IO uint32_t nTime); __IO uint8_t received_val = 0; int main(void) { SPIInit(); while(1) { while(!SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_RXNE)); received_val = SPI_I2S_ReceiveData(SPI2); } } void SPIInit(void){ GPIO_InitTypeDef GPIO_InitStruct; SPI_InitTypeDef SPI_InitStruct; RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB | RCC_AHB1Periph_GPIOE , ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15 ; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStruct.GPIO_OType = GPIO_OType_PP; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOB, &GPIO_InitStruct); GPIO_PinAFConfig(GPIOB, GPIO_PinSource13, GPIO_AF_SPI2); GPIO_PinAFConfig(GPIOB, GPIO_PinSource14, GPIO_AF_SPI2); GPIO_PinAFConfig(GPIOB, GPIO_PinSource15, GPIO_AF_SPI2); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_7 ; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStruct.GPIO_OType = GPIO_OType_PP; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOE, &GPIO_InitStruct); SPI_InitStruct.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStruct.SPI_Mode = SPI_Mode_Slave; SPI_InitStruct.SPI_DataSize = SPI_DataSize_8b; SPI_InitStruct.SPI_CPOL = SPI_CPOL_Low; SPI_InitStruct.SPI_CPHA = SPI_CPHA_1Edge; SPI_InitStruct.SPI_NSS = SPI_NSS_Hard; SPI_InitStruct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_256; SPI_InitStruct.SPI_FirstBit = SPI_FirstBit_MSB; SPI_Init(SPI2, &SPI_InitStruct); SPI_SSOutputCmd(SPI2, ENABLE); SPI_Cmd(SPI2, ENABLE); } I have made following connections Master (Discovery) - Slave (Discovery)
GND - GND PB13-PB13 (SCK) PB14-PB14 (MISO) PB15-PB15 (MOSI) PE7 - PE7 (Chip Select) Any help would be appreciated Thanks #spi-stm32f4-discovery-board
Labels:
- Labels:
-
SPI
0 REPLIES 0