2008-07-11 02:50 AM
Speech Codec AMR-WB on STM32F103ZE
2011-05-17 03:39 AM
I use the Ansi C Code from
http://www.3gpp1.org/ftp/specs/archive/26_series/26.173/ It is written as bit exakt without using of floating point numbers. (Fixed Point). I want to test the STM32 it this could be possible to run such a codec in a realtime application. do you speak german? hauschij@ba-loerrach.de2011-05-17 03:39 AM
Hi @all,
ich tried to run a speed codec AMR-WB on STM32F103ZE. Is there anybody who can give me an answer, if this could be possible. And perhaps is there somebody who can help me to optimize? i use the STM3210E-EVAL & Keil uVision3 & Keil ULINK2. why doesn't the keil compiler use the op-codes for the mac unit? my code is now running but it needs 240 msec. this is about 220 msec to long. thanks2011-05-17 03:39 AM
Hi hauschij,
What kind of software are you using? Are you using a free software from Internet? If yes, could you please tell me the source. Did Your code use the float lib? Why are using the wb (wideband) and not the narrowband? Are you planning to build a VoIP application? About Keil, try to disable the Micro Lib, this should improve the speed. What kind of optimizations you intend to do, maybe i can help you on this point. best regards sword2011-05-17 03:39 AM
Hi hauschij,
Since the code is based on fixed point arithmetic, you could run it easily on the STM32. But about the real time use, I think that this depends only on the CPU loading. So you must measure the encoding and decoding times to decide if you have to optimize some functions. Did you have a main with a simple implementation of encoding/decoding? I can help you by doing some benchmarks about the CPU loading and the functions that need to be optimized. But I need a ready project to start work on it. (Sorry I dont't speak german) Best regards sword