Posted on May 17, 2011 at 13:01Hello stm321, STM32 doesn't support USB OTG, it provides the device capability only. In other words, the STM32 cannot be a host it can be only a device! regards sword
Posted on May 17, 2011 at 12:50Hi all, kjepsen, The imaginary part of the input signal must be null. danielfpeixoto, I think you've made a small mistake: for each sample the real part is in the lowest 16-bit and the imaginary part is in the highest ...
Posted on May 17, 2011 at 12:39Hi utelettronico, According to my little knowldge about the MCU, it is not possible to stop an IP while debugging: so you cannot stop an ADC configured in continuous mode while debugging (I hope that I'm not talking no...