cancel
Showing results for 
Search instead for 
Did you mean: 

SPBT footprint

litteka
Associate
Posted on May 26, 2014 at 05:41

The SPBT2632C1A is the larger footprint, which is fine for our purposes.  

The datasheet does not make any mention of what the 6 extra pads on the bottom are for, yet there is a warning that

''thou shalt not ground extra pins'' and ''thou shalt ground Ground pins''.    The app note material for the SPBT2632C2A shows that there are 6 pins allocated to JTAG, so one might guess this is the case for the C1A as well, but can we confirm this please?

#spbt2632-bluetooth-footprint
1 REPLY 1
Amel NASRI
ST Employee
Posted on May 26, 2014 at 15:25

Sorry Arnim, but here we deal only with STM32 related topics.

Try to submit the same request in ''

https://my.st.com/public/STe2ecommunities/interface/Lists/Low%20Power%20RF%20Solutions/AllItems.aspx

'' forum, there you may find the right support you deserve.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.