cancel
Showing results for 
Search instead for 
Did you mean: 

source for TIMx UEV

dibs
Associate II
Posted on October 28, 2013 at 22:49

STM32F407xx

What are the sources for a TIMx update event?

My specific use case is that I am using TIM3 to generate a quadrature encoder output (CC1 and CC2). See the earlier discussion on how to do this: (quadrature output - STM32F407).  I am using an internal trigger to clock TIM1. TIM1 is set up to output a PWM signal based upon its input clock (TIM3). When I set CC1 as the trigger source, the output frequency from TIM1 is what I expect, but when I use the Update Event, it is doubled. This leads me to believe that I am either doing it wrong, and/or more than just the CNT=ARR generates an UEV.

Any thoughts?

#timer #stm32f4 #uev
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on October 29, 2013 at 00:13

[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/quadrature%20output%20-%20STM32F407&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=115]quadrature output - STM32F407 - cite

Well the toggle mode runs at 2x the frequency, is that what you mean? That's what allows the relative phase shift.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
Posted on October 29, 2013 at 09:31

It's a rising edge of the trigger which advances the slave timer. If the master's CC mode is toggle, it generates a rising edge only once per two periods of the master timer; whereas the update is a *pulse* one timer cycle long, generated at each overflow of the timer, it means a rising edge at every period of the master timer.

JW

dibs
Associate II
Posted on October 31, 2013 at 03:25

Thanks Jan,

Your answer makes sense based upon what I was seeing. Have you seen documentation that says this?