cancel
Showing results for 
Search instead for 
Did you mean: 

Some examples on the STM32CubeN6 SDK do not compile

wes_fflores
Visitor

Hello,

I am trying to compile some USB examples for the Nucleo-STM32N657X0-Q board that is available with the STM32CubeN6, but they are failing.

All USB examples at this location do not compile with IAR

STM32Cube_FW_N6_V1.0.0\Projects\NUCLEO-N657X0-Q\Applications\USBX

It seems to be related with the following library(USBPDCORE_NOPD_CM55_wc32.a) adding FPU instructions, when the MCU does not support it.

Is there an updated version for the STM32CubeN6 SDK that solves this problem?

Regards,

wes_fflores

1 REPLY 1
STTwo-32
ST Employee

Hello @wes_fflores 

I've test it personally using the IAR V9.50.2. Opening the project directly from Repository\STM32Cube_FW_N6_V1.0.0\Projects\NUCLEO-N657X0-Q\Applications\USBX\Ux_Device_CDC_ACM\EWARM\Project.eww and compile it does not show any error. 

Could you please confirm and send a screenshot of your error and the Tools you are using (if you are using CubeMX or not).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.