2014-09-03 2:55 PM
Hi,
I'm trying to modify the standard One Pulse example to use TIM15 to generate a delay, programmable width pulse, triggered by an external input. For the external input, I am using TIM3 routed to the appropriate pin (PA3) which is TIM15_CH2. I am looking at TIM15_CH1. The TIM3 output is working, generating an ~45 Hz trigger signal. However, I cannot get anything on the output of TIM15_CH1 (on PA2). Here is my code for TIM15:
static void TIM_Config(void)
{
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_ICInitTypeDef TIM_ICInitStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
/* TIM15 clock enable */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM15, ENABLE);
/* GPIOA clock enable */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
/* TIM15_CH1 pin (PA.02) and TIM15_CH2 pin (PA.03) configuration */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Connect TIM pins to AF0 */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_0);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_0);
/* --------------------------------------------------------------------------
TIM15 configuration: One Pulse mode
The external signal is connected to TIM15_CH2 pin (PA03),
The Rising edge is used as active edge,
The One Pulse signal is output on TIM15_CH1 pin (PA02)
The TIM_Pulse defines the delay value
The (TIM_Period - TIM_Pulse) defines the One Pulse value.
--------------------------------------------------------------------------- */
/* Compute the prescaler value */
PrescalerValue = (uint16_t) ((SystemCoreClock ) / 24000000) - 1;
/* Time base configuration */
TIM_TimeBaseStructure.TIM_Period = 65535;
TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM15, &TIM_TimeBaseStructure);
/* TIM15 PWM2 Mode configuration: Channel1 */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM2;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = 16383;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OC1Init(TIM15, &TIM_OCInitStructure);
/* TIM configuration in Input Capture Mode */
TIM_ICStructInit(&TIM_ICInitStructure);
TIM_ICInitStructure.TIM_Channel = TIM_Channel_2;
TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising;
TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI;
TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1;
TIM_ICInitStructure.TIM_ICFilter = 0;
TIM_ICInit(TIM15, &TIM_ICInitStructure);
/* One Pulse Mode selection */
TIM_SelectOnePulseMode(TIM15, TIM_OPMode_Single);
/* Input Trigger selection */
TIM_SelectInputTrigger(TIM15, TIM_TS_TI2FP2);
/* Slave Mode selection: Trigger Mode */
TIM_SelectSlaveMode(TIM15, TIM_SlaveMode_Trigger);
TIM_Cmd(TIM15, ENABLE);
}
It seems I am missing something - probably trivial! Any ideas?
Thanks!
2014-09-03 7:30 PM
Looks reasonable, but try clearing/setting all the parameters in the timebase. The repetition count is supported by TIM15, but not TIM2/TIM3
/* Time base configuration */
TIM_TimeBaseStructure.TIM_Period = 65535;
TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseStructure.TIM_RepetitionCounter = 0; // Used on TIM15
TIM_TimeBaseInit(TIM15, &TIM_TimeBaseStructure);
2014-09-04 5:22 AM
Good catch, but still, no joy.
Seems there are at least three possible problems:2014-09-04 11:21 AM
Did a bunch of double-checking, and I still cannot get any output. Checked connections, etc. Checked another board, nothing.
I recreated the example project, and it works fine using TIM2. Then, changed it to TIM15, and broken. Is it simply that TIM15 won't work that way??? For anyone interested in taking a whack at it, attached is the project. Ideas? ________________ Attachments : One_Pulse_TIM2_TIM15.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzwQ&d=%2Fa%2F0X0000000bRI%2Fut47qYfZ.QW59Xza28BXillR.hE2ajpRXH__lBREbwI&asPdf=false2014-09-05 12:11 AM
Try to make a ''conventional'' PWM working first on TIM15, then proceed to the triggered version.
Also, note, that TIM15 has the ''break'' unit at the outputs, i.e. the MOE bit in TIM15_BDTR has to be set (similar gotcha as with TIM1/TIM8 on the older STM32 models). If everything fails, read out and post content of TIM15 registers. JW2014-09-05 5:12 AM
Hey!
TIM15->BDTR |= TIM_BDTR_MOE;Works!Thank you, thank you, thank you!!!FWIW - no where in the reference manual did I see anything about this requirement; indeed, if anything, it seemed only to be applicable if the break feature is being used and enabled - which isn't my intent. Before writing this, though, I did a quick search and found ''Table 60 - Output control bits for complementary OCx and OCxN channels with break feature'' in RM0091, which states that when MOE is 0, ''Output Disabled (not driven by the timer)''. Thank the powers that be for the Internet, these forums, and mostly, people like waclawek.jan, clive1, and all the others that really make things run!2014-09-05 5:55 AM
Glad it works.
Note, that the code examples in Appendix A in RM0091 do mention it. They stem from the Snippets, which is IMO way more useful than the ''Standard Library'' crap perpetuated by the ''Cube'' crap. JW