cancel
Showing results for 
Search instead for 
Did you mean: 

[solved] MicroXplorer useless for STM32F050 TSSOP20..?

ffred
Associate II
Posted on December 15, 2013 at 14:23

Hello,

just tried MicroXplorer for a TSSOP20 STM32F050, but already un-installed it...

it didn't know the I2C interface !???

what's the point telling MicroXplorer support STM32F050 if he don't know the available peripherals ?

#microxplorer
3 REPLIES 3
Amel NASRI
ST Employee
Posted on December 16, 2013 at 14:04

Hello Ffred,

it didn't know the I2C interface !???

How exactly? If you are speaking about the ''Configuration'' tab, please note that only ''GPIO'' are supported in the current release.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

LaurentL
ST Employee
Posted on December 16, 2013 at 14:55

Hello ffred,

You are absolutely right the 3.2 version of MicroXplorer has some wrong pin definitions for some STM32F050 MCUs.

Please reinstall the software.

And unzip the attached file under the MicroXplorer installation directory to fix the issue.

Installation directory is C:\Program Files (x86)\STMicroelectronics\MicroXplorer under Windows 7 or C:\Program Files\STMicroelectronics\MicroXplorer under Windows XP.

Regards

Laurent

________________

Attachments :

pathDb.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Wp&d=%2Fa%2F0X0000000biC%2FkU8uhr48W_0KENr9Rx2vfF37WR77KQAs.9sgm.ucNQQ&asPdf=false
ffred
Associate II
Posted on December 16, 2013 at 19:11

Hi Laurent,

thanks a lot, it's working now !

ffred