2013-12-15 5:23 AM
Hello,
just tried MicroXplorer for a TSSOP20 STM32F050, but already un-installed it... it didn't know the I2C interface !??? what's the point telling MicroXplorer support STM32F050 if he don't know the available peripherals ? #microxplorer2013-12-16 5:04 AM
Hello Ffred,
it didn't know the I2C interface !???How exactly? If you are speaking about the ''Configuration'' tab, please note that only ''GPIO'' are supported in the current release.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2013-12-16 5:55 AM
Hello ffred,
You are absolutely right the 3.2 version of MicroXplorer has some wrong pin definitions for some STM32F050 MCUs. Please reinstall the software. And unzip the attached file under the MicroXplorer installation directory to fix the issue. Installation directory is C:\Program Files (x86)\STMicroelectronics\MicroXplorer under Windows 7 or C:\Program Files\STMicroelectronics\MicroXplorer under Windows XP. Regards Laurent ________________ Attachments : pathDb.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Wp&d=%2Fa%2F0X0000000biC%2FkU8uhr48W_0KENr9Rx2vfF37WR77KQAs.9sgm.ucNQQ&asPdf=false2013-12-16 10:11 AM
Hi Laurent,
thanks a lot, it's working now ! ffred