2020-03-26 12:31 AM
I am developping a touch screen user interface to control an audio preampl and dac.
I have no problems with I2C bus to set the registers of CT7302PL and ES9018K2M but if I try to read a single register the application hang.
This is my I2C configuration.
//######################################################################################
//# DAC SECTION
//######################################################################################
void SetReg_ES9018K2M()
{
unsigned char reg7, reg11;
BSP_I2C_Write(0x90, 8, 0b10011001); // GPIO1 & GPIO2 as INPUT based on reg#21
switch (inputsel)
{
case 0:
//write_ext_eeprom( 1,0b10001100); old ?
BSP_I2C_Write(0x90, 1, 0b10000100);
BSP_I2C_Write(0x90, 21, 0b00000000);
BSP_I2C_Write(0x90, 11, 0b00000000);
break;
case 1:
BSP_I2C_Write(0x90, 1, 0b10000001);
BSP_I2C_Write(0x90, 21, 0b01010000);
BSP_I2C_Write(0x90, 11, 0b00110000); // 3
break;
case 2:
BSP_I2C_Write(0x90, 1, 0b10000001);
BSP_I2C_Write(0x90, 21, 0b01010000);
BSP_I2C_Write(0x90, 11, 0b01000000); // 4
break;
}
reg11 = BSP_I2C_Read(0x90, 11);
}
void BSP_I2C_Init()
{
#define I2C_ADDRESS 0x3c
#define I2C_TIMING 0x00B1112E
hi2c1.Instance = I2C1;
hi2c1.Init.Timing = I2C_TIMING;
hi2c1.Init.OwnAddress1 = I2C_ADDRESS;
hi2c1.Init.OwnAddress1 = 0x78; // an unused address
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
I2Cx_Init(&hi2c1);
}
2020-03-26 8:53 AM
Solved with these functions instead of BSP_I2C_...
CAMERA_IO_Init();
CAMERA_IO_Write(0x90, 8, 0b10011001);
CAMERA_IO_Read(0x90, 64);
2020-03-28 7:50 AM
Solved all I2C lock with 3 action on STM32F746-DISCO:
1) pull-up resistors 4700ohm to 3.3V on both SDA and SCL wire
2) Use CAMERA_IO_Init, Read and Write instead of BSP_I2S_Init, Reda and Write
3) Using the EXT/RF E2P connector (pin EXT_SDA/EXT_SCL) instead of CN7 connector (pin SDA/SCL)
The lock was inside this function:
static HAL_StatusTypeDef I2C_WaitOnFlagUntilTimeout(I2C_HandleTypeDef *hi2c, uint32_t Flag, FlagStatus Status, uint32_t Timeout, uint32_t Tickstart)
{
int i = 0;
while (__HAL_I2C_GET_FLAG(hi2c, Flag) == Status)
{
#ifdef MY_TEST_TO_TRY_TO_UNLOCK
// Using this code the function return the error without lock the my app
// but I don't know how to recognize the error condition in the CAMERA_IO_Read()
if (i < 60000)
i++;
else
{
hi2c->ErrorCode |= HAL_I2C_ERROR_TIMEOUT;
hi2c->State = HAL_I2C_STATE_READY;
hi2c->Mode = HAL_I2C_MODE_NONE;
__HAL_UNLOCK(hi2c);
return HAL_ERROR;
}
#endif
#ifdef ORIGINAL
/* Check for the Timeout */
if (Timeout != HAL_MAX_DELAY)
{
if (((HAL_GetTick() - Tickstart) > Timeout) || (Timeout == 0U))
{
hi2c->ErrorCode |= HAL_I2C_ERROR_TIMEOUT;
hi2c->State = HAL_I2C_STATE_READY;
hi2c->Mode = HAL_I2C_MODE_NONE;
/* Process Unlocked */
__HAL_UNLOCK(hi2c);
return HAL_ERROR;
}
}
#endif
}
return HAL_OK;
}