2014-05-06 03:38 AM
Hi all,
I'm working on the example using the
Omnivision camera ov2640, but I'm not sure about the
resolution of the image coming from the camera.
I would like to configure the camera with QQVGA resolution(160x120).
I have done this configuration :
const
unsigned
char
OV2640_QQVGA[][2]=
{
{0xff, 0x00},
{0x2c, 0xff},
{0x2e, 0xdf},
{0xff, 0x01},
{0x3c, 0x32},
{0x11, 0x00},
{0x09, 0x02},
{0x04, 0xA8},
{0x13, 0xe5},
{0x14, 0x48},
{0x2c, 0x0c},
{0x33, 0x78},
{0x3a, 0x33},
{0x3b, 0xfB},
{0x3e, 0x00},
{0x43, 0x11},
{0x16, 0x10},
{0x4a, 0x81},
{0x21, 0x99},
{0x24, 0x40},
{0x25, 0x38},
{0x26, 0x82},
{0x5c, 0x00},
{0x63, 0x00},
{0x46, 0x3f},
{0x0c, 0x3c},
{0x61, 0x70},
{0x62, 0x80},
{0x7c, 0x05},
{0x20, 0x80},
{0x28, 0x30},
{0x6c, 0x00},
{0x6d, 0x80},
{0x6e, 0x00},
{0x70, 0x02},
{0x71, 0x94},
{0x73, 0xc1},
{0x3d, 0x34},
{0x5a, 0x57},
{0x12, 0x00},
//UXGA
{0x11, 0x00},
{0x17, 0x11},
{0x18, 0x75},
{0x19, 0x01},
{0x1a, 0x97},
{0x32, 0x36},
{0x03, 0x0f},
{0x37, 0x40},
{0x4f, 0xbb},
{0x50, 0x9c},
{0x5a, 0x57},
{0x6d, 0x80},
{0x6d, 0x38},
{0x39, 0x02},
{0x35, 0x88},
{0x22, 0x0a},
{0x37, 0x40},
{0x23, 0x00},
{0x34, 0xa0},
{0x36, 0x1a},
{0x06, 0x02},
{0x07, 0xc0},
{0x0d, 0xb7},
{0x0e, 0x01},
{0x4c, 0x00},
{0xff, 0x00},
{0xe5, 0x7f},
{0xf9, 0xc0},
{0x41, 0x24},
{0xe0, 0x14},
{0x76, 0xff},
{0x33, 0xa0},
{0x42, 0x20},
{0x43, 0x18},
{0x4c, 0x00},
{0x87, 0xd0},
{0x88, 0x3f},
{0xd7, 0x03},
{0xd9, 0x10},
{0xd3, 0x82},
{0xc8, 0x08},
{0xc9, 0x80},
{0x7d, 0x00},
{0x7c, 0x03},
{0x7d, 0x48},
{0x7c, 0x08},
{0x7d, 0x20},
{0x7d, 0x10},
{0x7d, 0x0e},
{0x90, 0x00},
{0x91, 0x0e},
{0x91, 0x1a},
{0x91, 0x31},
{0x91, 0x5a},
{0x91, 0x69},
{0x91, 0x75},
{0x91, 0x7e},
{0x91, 0x88},
{0x91, 0x8f},
{0x91, 0x96},
{0x91, 0xa3},
{0x91, 0xaf},
{0x91, 0xc4},
{0x91, 0xd7},
{0x91, 0xe8},
{0x91, 0x20},
{0x92, 0x00},
{0x93, 0x06},
{0x93, 0xe3},
{0x93, 0x02},
{0x93, 0x02},
{0x93, 0x00},
{0x93, 0x04},
{0x93, 0x00},
{0x93, 0x03},
{0x93, 0x00},
{0x93, 0x00},
{0x93, 0x00},
{0x93, 0x00},
{0x93, 0x00},
{0x93, 0x00},
{0x93, 0x00},
{0x96, 0x00},
{0x97, 0x08},
{0x97, 0x19},
{0x97, 0x02},
{0x97, 0x0c},
{0x97, 0x24},
{0x97, 0x30},
{0x97, 0x28},
{0x97, 0x26},
{0x97, 0x02},
{0x97, 0x98},
{0x97, 0x80},
{0x97, 0x00},
{0x97, 0x00},
{0xc3, 0xef},
{0xff, 0x00},
{0xba, 0xdc},
{0xbb, 0x08},
{0xb6, 0x24},
{0xb8, 0x33},
{0xb7, 0x20},
{0xb9, 0x30},
{0xb3, 0xb4},
{0xb4, 0xca},
{0xb5, 0x43},
{0xb0, 0x5c},
{0xb1, 0x4f},
{0xb2, 0x06},
{0xc7, 0x00},
{0xc6, 0x51},
{0xc5, 0x11},
{0xc4, 0x9c},
{0xbf, 0x00},
{0xbc, 0x64},
{0xa6, 0x00},
{0xa7, 0x1e},
{0xa7, 0x6b},
{0xa7, 0x47},
{0xa7, 0x33},
{0xa7, 0x00},
{0xa7, 0x23},
{0xa7, 0x2e},
{0xa7, 0x85},
{0xa7, 0x42},
{0xa7, 0x33},
{0xa7, 0x00},
{0xa7, 0x23},
{0xa7, 0x1b},
{0xa7, 0x74},
{0xa7, 0x42},
{0xa7, 0x33},
{0xa7, 0x00},
{0xa7, 0x23},
{0xc0, 0xc8},
{0xc1, 0x96},
{0x8c, 0x00},
{0x86, 0x3d},
{0x50, 0x92},
{0x51, 0x90},
{0x52, 0x2c},
{0x53, 0x00},
{0x54, 0x00},
{0x55, 0x88},
{0x5a, 0x50},
{0x5b, 0x3c},
{0x5c, 0x00},
{0xd3, 0x04},
{0x7f, 0x00},
{0xda, 0x00},
{0xe5, 0x1f},
{0xe1, 0x67},
{0xe0, 0x00},
{0xdd, 0x7f},
{0x05, 0x00},
{0xff, 0x00},
{0xe0, 0x04},
{0xc0, 0xc8},
{0xc1, 0x96},
{0x86, 0x3d},
{0x50, 0x92},
{0x51, 0x90},
{0x52, 0x2c},
{0x53, 0x00},
{0x54, 0x00},
{0x55, 0x88},
{0x57, 0x00},
{0x5a, 0x28},
{0x5b, 0x1E},
{0x5c, 0x00},
{0xd3, 0x08},
//was 0x08
{0xe0, 0x00},
{0xFF, 0x00},
{0x05, 0x00},
{0xDA, 0x08},
{0xda, 0x09},
{0x98, 0x00},
{0x99, 0x00},
{0x00, 0x00},*/
};
but this configuration doesn't work well .It gives me 113 lines instead of 120 lines .There is something wrong in the configuration !!
Has anyone solved this question!
below is the datasheet of tha camera omnivision 2640
2014-05-06 05:55 AM
I'm testing with the OV7670 which is quite similar in the SCCB/I2C interface. I get too little number of lines only when the PCLK is too fast and I read out the cam too slow.
What happens if you set the PCLK prescaler to return less fps?2014-05-06 07:21 AM
Thank you for your answer 🙂
this is the code to set pclk at 272khz(slow mode)CAMERA_IO_Write(DeviceAddr, 0xff, 0x01);
CAMERA_IO_Write(DeviceAddr, 0x11, 0x20);
the number of lines =114<120 lines
2014-05-07 08:02 AM
2014-05-07 08:51 AM
I would be more confident in this measure when the scope capture shows both edges of the VSync signal.
Show us the capture that measures correctly the 240 lines in QVGA mode.