Skip to main content
veyselka
Associate II
August 29, 2014
Question

SMT32F4 Discovery CAN Example with Interrupt

  • August 29, 2014
  • 1 reply
  • 904 views
Posted on August 29, 2014 at 19:20

Hi everyone,

I need a help about CAN integration . I want to create a CAN network with using 2 STM32F discovery board. When I set STM32, CAN_Loopback mode, When I send data to CAN also I will reacive it form my CAN1 interrupt. Interrupts look like working , But I cant read all data which I send CAN1 interrupt handler - its only send data to serial port.

/**
* @brief This function handles CAN1 RX0 Handler.
* @param None
* @retval None
*/
void CAN1_RX0_IRQHandler(void)
{
CAN_Receive(CAN1, CAN_FIFO0, &RxMessage);
printf(''CAN_RX %04X - %02X - %02X %02X %02X %02X %02X %02X %02X %02X \r\n'',RxMessage.StdId,RxMessage.DLC,
RxMessage.Data[0],RxMessage.Data[1],RxMessage.Data[2],RxMessage.Data[3],
RxMessage.Data[4],RxMessage.Data[5],RxMessage.Data[6],RxMessage.Data[7]);
}

user button interrupt code is

void EXTI0_IRQHandler(void)
{
static int8_t data;
if(EXTI_GetITStatus(EXTI_Line0) != RESET)
{
/* Clear the EXTI line 0 pending bit */
EXTI_ClearITPendingBit(EXTI_Line0);
/* Toggle LED3 */
CAN_Tx_CMD(data); // SEND DATA to CAN NETWORK
toggle_led(LED2);
data++;
}
}

CAN Transmit code is just add one to data and my CAN data[0] will increase every button pressed

uint8_t CAN_Tx_CMD(int8_t data)
{
CanTxMsg TxMessage;
TxMessage.StdId = 0x0123;
TxMessage.ExtId = 0x0;
TxMessage.RTR = CAN_RTR_DATA;
TxMessage.IDE = CAN_ID_STD;
TxMessage.DLC = 1;
TxMessage.Data[0] = ((uint8_t)data);
TxMessage.Data[1] = ((uint8_t)0xFF);
TxMessage.Data[2] = ((uint8_t)0xFA);
TxMessage.Data[3] = ((uint8_t)0xFF);
TxMessage.Data[4] = ((uint8_t)0xFA);
TxMessage.Data[5] = ((uint8_t)0xFF);
TxMessage.Data[6] = ((uint8_t)0xFA);
TxMessage.Data[7] = ((uint8_t)0xFF);
CAN_Transmit(CAN1, &TxMessage);
if(CAN_TransmitStatus(CAN1, 0)==0){
printf(''TRANSMIT CAN ERROR\r\n'');
return 0;
}else{
return 1;
}
}

CAN init function is ( I think all problem could be in this)

void can_init(void)
{
CAN_InitTypeDef CAN_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
CAN_FilterInitTypeDef CAN_FilterInitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
/* CAN1 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1, ENABLE);
/* Init CAN GPIO clocks */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);
/* Connect CAN_RX & CAN_TX to AF9 */
GPIO_PinAFConfig(GPIOD, GPIO_PinSource0, GPIO_AF_CAN1); //CAN_RX = PB12
GPIO_PinAFConfig(GPIOD, GPIO_PinSource1, GPIO_AF_CAN1); //CAN_TX = PB13
/* Configure CAN RX and TX pins */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOD, &GPIO_InitStructure);
/* CAN1 reset */
CAN_DeInit(CAN1);
/* CAN2 configuration */
CAN_InitStructure.CAN_TTCM = DISABLE; // time-triggered communication mode = DISABLED
CAN_InitStructure.CAN_ABOM = DISABLE; // automatic bus-off management mode = DISABLED
CAN_InitStructure.CAN_AWUM = DISABLE; // automatic wake-up mode = DISABLED
CAN_InitStructure.CAN_NART = DISABLE; // non-automatic retransmission mode = DISABLED
CAN_InitStructure.CAN_RFLM = DISABLE; // receive FIFO locked mode = DISABLED
CAN_InitStructure.CAN_TXFP = DISABLE; // transmit FIFO priority = DISABLED
//CAN_InitStructure.CAN_Mode = CAN_Mode_Normal; // Debug can mode
CAN_InitStructure.CAN_Mode = CAN_Mode_LoopBack; // Debug can mode
CAN_InitStructure.CAN_SJW = CAN_SJW_1tq; // synchronization jump width = 1
CAN_InitStructure.CAN_BS1 = CAN_BS1_12tq; //10
CAN_InitStructure.CAN_BS2 = CAN_BS2_2tq; //4
CAN_InitStructure.CAN_Prescaler = 6; // baudrate 500 kbps APB1 = 45MHz tq + tq*BS1 + tq*BS2 73%
CAN_Init(CAN1, &CAN_InitStructure);
/* Default filter - accept all to CAN_FIFO*/
CAN_InitStructure.CAN_Mode = CAN_OperatingMode_Initialization; // Can to init mode
CAN_FilterInitStructure.CAN_FilterActivation = DISABLE; // Disable filter
CAN_FilterInitStructure.CAN_FilterNumber = 0; // 0..13 for CAN1, .27 for CAN2
CAN_FilterInitStructure.CAN_FilterFIFOAssignment = CAN_FIFO0;
CAN_FilterInitStructure.CAN_FilterMode = CAN_FilterMode_IdMask;
CAN_FilterInitStructure.CAN_FilterScale = CAN_FilterScale_16bit;
CAN_FilterInitStructure.CAN_FilterIdHigh = 0x0000;
CAN_FilterInitStructure.CAN_FilterIdLow = 0x0000;
CAN_FilterInitStructure.CAN_FilterMaskIdHigh = 0x0000;
CAN_FilterInitStructure.CAN_FilterMaskIdLow = 0x0000;
CAN_FilterInitStructure.CAN_FilterFIFOAssignment = 0;
CAN_FilterInitStructure.CAN_FilterActivation = ENABLE;
CAN_FilterInit(&CAN_FilterInitStructure);
// CAN INTERRUPT Configration
NVIC_InitStructure.NVIC_IRQChannel = CAN1_RX0_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
CAN_ITConfig(CAN1, CAN_IT_FMP0, ENABLE);
}

So , When I pressed user button , my serial output is like CAN_RX 0123 - 01 - 00 00 00 00 00 00 00 00 CAN_RX 0123 - 01 - 01 00 00 00 00 00 00 00 CAN_RX 0123 - 01 - 02 00 00 00 00 00 00 00 CAN_RX 0123 - 01 - 03 00 00 00 00 00 00 00 Why RxMessage[1] -- [7] is 00 , It has to be FF FA FF FA .. Best Regards #stm32f4 #can #discovery
This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
August 29, 2014
Posted on August 29, 2014 at 20:31

Why RxMessage[1] -- [7] is 00 , It has to be FF FA FF FA ..

TxMessage.DLC = 1;

//?????!
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..