2014-08-27 2:37 PM
Is there any reason why I could not (or you recommend to not) short the Vcc (pin 1&2) and Vdd (pin 19) lines on the ST-Link/V2 programmer during development? I would prefer to power the target application board, via the programmer, during development to eliminate the need for an external power supply.
Thanks2014-08-27 7:13 PM
Just be cautious, the pin 19 usage is a non-standard, and SEGGER's J-Link pushes out 5V on this pin.
2014-08-29 2:56 PM
Great, thanks, Clive.