cancel
Showing results for 
Search instead for 
Did you mean: 

Slave mode trigger on STM32F411RE

christophe2
Associate II
Posted on September 02, 2015 at 15:38

Hi,

I'm trying to enable the timer 2 on a rising edge of a signal that i have

connect on the tim2_ch1. I understand that the slave trigger mode of the timer

can do that. I want to generate a signal on the tim2_ch2 on the rising edge of

the tim2_ch1.

Additionally, I would like to generate another signal on tim3_ch2 on

the rising edge of the tim2_ch2.

I did that by connecting the tim2 and tim3 as master and slave and it's worked.

But the tim2_ch2 is generated before the rising edge of the tim2_ch1.

Is it possible to start a counter on an external trigger or i have missed something?

I've copied my program below :

   

TimHandle.Instance = TIM2;

  TimHandle.Init.ClockDivision = 0;

  TimHandle.Init.CounterMode = TIM_COUNTERMODE_UP;

  TimHandle.Init.Period =  10; //Compteur_SCK

  TimHandle.Init.Prescaler = 0;

  TimHandle.Init.RepetitionCounter = 0;

  ocConfig.OCMode = TIM_OCMODE_TOGGLE;

  ocConfig.OCPolarity = TIM_OCPOLARITY_HIGH;

  icConfig.ICFilter         = 1;

  icConfig.ICPolarity         = TIM_ICPOLARITY_RISING;

  icConfig.ICPrescaler         = TIM_ICPSC_DIV1;

  icConfig.ICSelection         = TIM_ICSELECTION_DIRECTTI;

  if(HAL_TIM_OC_Init(&TimHandle) != HAL_OK)

  {

    Error_Handler();

  }

  if(HAL_TIM_OC_ConfigChannel(&TimHandle,&ocConfig,TIM_CHANNEL_2) != HAL_OK)

  {

    Error_Handler();

  }

  if(HAL_TIM_IC_ConfigChannel(&TimHandle,&icConfig,TIM_CHANNEL_1) != HAL_OK)

  {

    Error_Handler();

  }

  slaveConfig.InputTrigger = TIM_TS_TI1FP1;

  slaveConfig.SlaveMode = TIM_SLAVEMODE_TRIGGER;

  slaveConfig.TriggerFilter = 1;

  slaveConfig.TriggerPolarity = TIM_TRIGGERPOLARITY_RISING;

  slaveConfig.TriggerPrescaler = TIM_TRIGGERPRESCALER_DIV1;

  if( HAL_TIM_SlaveConfigSynchronization(&TimHandle,&slaveConfig) != HAL_OK)

  {

    Error_Handler();

  }

  masterConfig.MasterOutputTrigger =  TIM_TRGO_OC2REF;

  masterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_ENABLE;

  if(HAL_TIMEx_MasterConfigSynchronization(&TimHandle,&masterConfig) != HAL_OK)

  {

    Error_Handler();

  }

  /////////////////////////////////////////////////////////////////////////////////

  /////////////////////////////////////////////////////////////////////////////////

  Tim2Handle.Instance = TIM3;

  Tim2Handle.Init.ClockDivision = 0;

  Tim2Handle.Init.CounterMode = TIM_COUNTERMODE_UP;

  Tim2Handle.Init.Period = 2000;

  Tim2Handle.Init.Prescaler = 0;

  oc2Config.OCMode = TIM_OCMODE_PWM1;

  oc2Config.OCPolarity = TIM_OCPOLARITY_HIGH;

  oc2Config.Pulse     = 20;

  if(HAL_TIM_OC_Init(&Tim2Handle) != HAL_OK)

  {

    Error_Handler();

  }

  if(HAL_TIM_PWM_ConfigChannel(&Tim2Handle,&oc2Config,TIM_CHANNEL_2) != HAL_OK)

  {

    Error_Handler();

  }

  if(HAL_TIM_IC_ConfigChannel(&Tim2Handle,&icConfig,TIM_CHANNEL_1) != HAL_OK)

  {

    Error_Handler();

  }

  slaveConfig.InputTrigger = TIM_TS_ITR1;

  slaveConfig.SlaveMode = TIM_SLAVEMODE_TRIGGER;

  slaveConfig.TriggerFilter = 1;

  slaveConfig.TriggerPolarity = TIM_TRIGGERPOLARITY_RISING;

  slaveConfig.TriggerPrescaler = TIM_TRIGGERPRESCALER_DIV1;

  if( HAL_TIM_SlaveConfigSynchronization(&Tim2Handle,&slaveConfig) != HAL_OK)

  {

      Error_Handler();

  }

  if(HAL_TIM_IC_Start(&TimHandle,TIM_CHANNEL_1) != HAL_OK)

  {

  Error_Handler();

  }

  if(HAL_TIM_IC_Start(&Tim2Handle,TIM_CHANNEL_1) != HAL_OK)

  {

  Error_Handler();

  }

  if(HAL_TIM_OC_Start(&TimHandle,TIM_CHANNEL_2) != HAL_OK)

  {

    Error_Handler();

  }

  if(HAL_TIM_OC_Start(&Tim2Handle,TIM_CHANNEL_2) != HAL_OK)

  {

      Error_Handler();

  }

Thanks for your help, sorry for my english..

#trigger #timer #stm32f4
4 REPLIES 4
Posted on September 02, 2015 at 18:26

Your english is OK, what I don't understand is the Cube gibberish.

Post the content of relevant registers, including registers for the GPIO pin you use as external trigger.

JW

christophe2
Associate II
Posted on September 03, 2015 at 11:02

Thanks for your answer,

I've copied some registers values, I hope it helps to find the solution,

I can provide more values if you need.

The pins which are used for TIM1 are :

tim1_ch1 : PA8

tim1_ch2 : PA9

tim2_ch1 : PA0

tim2_ch2 : PA1

Timer 1 Register :

BDTR : MOE = 1 (Main Output Enable)

CCER : CC1E = 1 (Capture enable)

              CC2E = 1 (Compare enable)

CCMR1_Input : CC1S = 1 (CC1 Channel configure as input, IC1 mapped on TI1)

CCMR1_Output : CC1S  = 1 (CC1 Channel configure as input, IC1 mapped on TI1 )                            

OC1M  = 1 (Set channel 1 to active level on match)

                            OC2M  = 3 (OC2REF toggle when CNT = CCR)

CR1 : CEN = 1 (Counter enable)

CR2 : MMS = 5 ( OC2REF is used a signal trigger output)

SMCR : MSM = 1 ( Master Slave mode enabled)

               SMS = 6 ( slave Trigger mode)

                  TS = 5  ( Filtered timer input 1)

GPIOA Register

:

MODER : MODER0  = 2 (Alternate function mode)

                  MODER1  = 2

                  MODER8  = 2

                  MODER9  = 2

PUPDR : PUPDR0 = 0 (AF0 is selected)

                PUPDR1 = 0 

                PUPDR8 = 0 

                PUPDR9 = 0

Posted on September 03, 2015 at 11:44

> I can provide more values if you need.

I don't need them - it's YOU who needs them! :)

1. GPIOA->AFRL/AFRH?

2. Once TIM1->CR1.EN is set, there's no point in triggering - the only thing the trigger does is it *sets* CR1.EN, never resets it.

This kind of problems can be effectively debugged directly by writing/observing registers in the debugger. First, get the capture working - set the timer to free running, set GPIO appropriately, enable capture, then externally toggle the pin's level and observe changes in the capture register.

JW

christophe2
Associate II
Posted on September 03, 2015 at 15:23

I have found the problem by doing step by step and observing the registers values.

CR1.EN was enabled before the capture on channel 1 and others values like MOE

and CC1E was not properly set.

Thanks a lot for your support :)