Since the PIN of STSPIN32F0 is not enough, it is implemented to view log messages using PA14 (SWD_CLK) as UART.
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-04-17 9:14 PM
Since the PIN of STSPIN32F0 is not enough, it is implemented to view log messages using PA14 (SWD_CLK) as UART.
But after that, I can't download it, so please inquire.
1. Could you explain that re-download the MCU in this state?
2. I don't have any PIN, so if there is a way or example to use PA14 as a UART and download it again, I would like to ask if it is possible to share.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-04-18 6:29 AM
PA14 is used for SWD. If you've repurposed it for another use, you can't connect with SWD. You can boot up into the bootloader or use Connect Under Reset to recover the chip.
If you feel a post has answered your question, please click "Accept as Solution".