cancel
Showing results for 
Search instead for 
Did you mean: 

Simpler uC with CAN feature

zpedro
Associate

Hello community!

What are the simplest ST uC with CAN feature?

Yours suggestions will be welcome!

Many thanks and Regards!

 

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello @zpedro and welcome to the community,

That depends on what do you mean by "the simplest ST uC".

First, there are two CAN flavors: bxCAN peripheral (CAN2.0) and FDCAN peripheral (CANFD).

Second, STM32F0, STM32F1, STM32F2, STM32F3, STM32F4, STM32F7 families have bxCAN peripheral

while STM32G4, STM32H7, STM32H5 etc .. have FDCAN peripheral.

So if you mean by simple not a very complex MCU I can suggest STM32F0 family based on Cortex-M0:

You can use STM32CUbeMx or STM32Finder tools to select the suitable MCU for your application:

SofLit_0-1739188147485.png

Hope that helps.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
mƎALLEm
ST Employee

Hello @zpedro and welcome to the community,

That depends on what do you mean by "the simplest ST uC".

First, there are two CAN flavors: bxCAN peripheral (CAN2.0) and FDCAN peripheral (CANFD).

Second, STM32F0, STM32F1, STM32F2, STM32F3, STM32F4, STM32F7 families have bxCAN peripheral

while STM32G4, STM32H7, STM32H5 etc .. have FDCAN peripheral.

So if you mean by simple not a very complex MCU I can suggest STM32F0 family based on Cortex-M0:

You can use STM32CUbeMx or STM32Finder tools to select the suitable MCU for your application:

SofLit_0-1739188147485.png

Hope that helps.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hi SofLit, many thanks for the tip! ;)

Regards,

José