cancel
Showing results for 
Search instead for 
Did you mean: 

Setting up HyperRAM S70KL1282 with STM32H735 issues

MartinDQ
Associate III

Hi,

I'm trying to setup this new RAM chips on STM32H735 in OSPI/HyperRAM mode. The HW connection is the same as on ST STM32H735 devkit. I found a driver for similar chip S70KL1281 but there are some differences, e.g. in latencies, but generally S70KL1282 is faster. The used driver file identification from header:

******************************************************************************
* @file s70kl1281.c
* @modify MCD Application Team
* @brief This file provides the S70KL1281 OSPI drivers.

...

* Copyright (c) 2020 STMicroelectronics.
******************************************************************************

I configured the Hyperbus in STM32CubeMX but there are no hints how to setup all the options for this memory. So after some messing and trial-error I ended with this partially working init code:

 

 

static void MX_OCTOSPI2_Init(void)
{
  OSPIM_CfgTypeDef sOspiManagerCfg = {0};
  OSPI_HyperbusCfgTypeDef sHyperBusCfg = {0};

  /* OCTOSPI2 parameter configuration*/
  hospi2.Instance = OCTOSPI2;
  hospi2.Init.FifoThreshold = 1;
  hospi2.Init.DualQuad = HAL_OSPI_DUALQUAD_DISABLE;
  hospi2.Init.MemoryType = HAL_OSPI_MEMTYPE_HYPERBUS;
  hospi2.Init.DeviceSize = 24;
  hospi2.Init.ChipSelectHighTime = 1;
  hospi2.Init.FreeRunningClock = HAL_OSPI_FREERUNCLK_DISABLE;
  hospi2.Init.ClockMode = HAL_OSPI_CLOCK_MODE_0;
  hospi2.Init.WrapSize = HAL_OSPI_WRAP_NOT_SUPPORTED;
  hospi2.Init.ClockPrescaler = 2; // for testing use prescaler 2 at 133MHz, prescaler 1 gets garbage
  hospi2.Init.SampleShifting = HAL_OSPI_SAMPLE_SHIFTING_NONE;
  hospi2.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_ENABLE;
  hospi2.Init.ChipSelectBoundary = 0;
  hospi2.Init.DelayBlockBypass = HAL_OSPI_DELAY_BLOCK_USED;
  hospi2.Init.MaxTran = 0;
  hospi2.Init.Refresh = 500;
  if (HAL_OSPI_Init(&hospi2) != HAL_OK)
  {
    Error_Handler();
  }
  sOspiManagerCfg.ClkPort = 2;
  sOspiManagerCfg.DQSPort = 2;
  sOspiManagerCfg.NCSPort = 2;
  sOspiManagerCfg.IOLowPort = HAL_OSPIM_IOPORT_2_LOW;
  sOspiManagerCfg.IOHighPort = HAL_OSPIM_IOPORT_2_HIGH;
  if (HAL_OSPIM_Config(&hospi2, &sOspiManagerCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
  {
    Error_Handler();
  }
  sHyperBusCfg.RWRecoveryTime = 3;
  sHyperBusCfg.AccessTime = 7;
  sHyperBusCfg.WriteZeroLatency = HAL_OSPI_NO_LATENCY_ON_WRITE; // someone suggested HAL_OSPI_LATENCY_ON_WRITE but doesn't have effect
  sHyperBusCfg.LatencyMode = HAL_OSPI_FIXED_LATENCY;
  if (HAL_OSPI_HyperbusCfg(&hospi2, &sHyperBusCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
  {
    Error_Handler();
  }
}

 

 

First time I had a problem that reading from memory was unrealiable and I sometimes getting a different results on every run. Enabling the magic option hospi2.Init.DelayBlockBypass = HAL_OSPI_DELAY_BLOCK_USED; solved it but still not at the full clock speed I configured - I have both OSPI clocked at 133MHz. The FlashROM at OSPI1 works fine at 133MHz but for this HyperRAM I have to set prescaler 2. Then I got some consistent result.

But there's another problem that test data pattern I wrote into memory are readed by 8 Bytes shifted further than it should be. Currently for testing I don't use mapping yet but I use driver functions S70KL1281_Write and S70KL1281_Read. A simple piece of code for test write and readbeck:

 

 

{
uint8_t buff[64]={0};
int i;
buff[0]=0xab; buff[1]=0xcd; buff[2]=0xef; buff[3]=0xaa;
if (S70KL1281_Write(&XRAM, buff, 0, 16)!=S70KL1281_OK)
  printf("Failed to write to HyperRAM\n");
for (i=0; i<32; i++)
  printf("%02X ", buff[i]);
printf("\n");
if (S70KL1281_Read(&XRAM, buff, 0, 32)!=S70KL1281_OK)
  printf("Failed to read from HyperRAM\n");
for (i=0; i<32; i++)
  printf("%02X ", buff[i]);
printf("\n");
if (S70KL1281_Read(&XRAM, buff, 0, 32)!=S70KL1281_OK)
  printf("Failed to read from HyperRAM\n");
for (i=0; i<32; i++)
  printf("%02X ", buff[i]);
printf("\n");
}

 

 

The memory address is 0 but I get this:

Ext. OctoSPI HyperRAM ID: 0C81 0001
Manufacturer: Infineon, HyperRAM 2.0, rowbits: 13, colbits: 9
AB CD EF AA 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
57 47 57 5D D5 D7 8C 15 AB CD EF AA 00 00 00 00 00 00 00 00 00 00 00 00 D5 D5 57 5F D5 D5 5F 75
57 47 57 5D D5 D7 8C 15 AB CD EF AA 00 00 00 00 00 00 00 00 00 00 00 00 D5 D5 57 5F D5 D5 5F 75

There's some garbage in first 8 Bytes (57 47 57 5D D5 D7 CC 15 - uninitialized memory?) followed by correct pattern AB CD EF AA and trailing zeros from buffer

22 REPLIES 22

I tried to vary hospi2.Init.Refresh with different values: 50, 100, 200, 300, 500, 1000 and it doesn't have any effect on 8-byte data write offset. I think it doesn't matter anyway because I write only a short data block that's transfered many times faster than the refresh interval...

MartinDQ
Associate III

Any chance that some engineer from ST could try the new memory S70KL1282 on the discovery kit?

I think that they will be forced to upgrade anyway as the current part is EoL and will be no longer available. Except they bought a huge amount of old chips so they still have enough spare...

LCE
Principal

So it's still not working?

I just got the message that will get my prototypes with the S70KL1282 in mid / end june.

MartinDQ
Associate III

No, refresh settings didn't have any effect on this issue. Currently I'm working on other project so I'll return to this later. I also asked on Infineon forum where they only suggested a change of latency 6->7 that I already did...

Hello @MartinDQ 

 
Currently, the S70KL1282 is not available at my end. However, I will inquire further internally and provide you with an update as soon as possible.
 
Kind regards,
Nissrine. 
rk_iot
Associate II

Hello @NEL M.1 

 

do you have any updates on that issue? We are planning to use the S70KL1282 with the STM32H735 for our product, and are concerned that we could not make the HyperRAM work properly, which would be critical for our design.

 

Thanks and kind regards,

RK_IOT 

LCE
Principal

@MartinDQ & @NEL M.1 

I'm also curious...

@rk_iot 
I'll get some custom boards with H733 + S70KL1282 in June, then I will be able to test.

The good thing: there are a few pin-compatible octal SPI / HyperRam devices available from other companies.
But I hope it will be possible to make it work...  

MartinDQ
Associate III

Hi, sorry, I'm currently working on another PCB design project so I didn't debug it further. But I got some sample code from Infineon for this memory chip and a bit different STM32 MCU that is claimed to work. I hope I'll have a time to try it out soon, I'll post the result here too.

Hello @rk_iot , @MartinDQ 

I have not received the sample yet, but I will keep you updated once I test it.

In the meantime, @MartinDQ, have you checked that all the signals have the same length ?

You can check the following thread:  Solved: Write/Read issues with HyperRAM S70KL1282 on OctoS... - STMicroelectronics Community. It may help you.

 

Kind regards

MartinDQ
Associate III

Yes I did take a care about QSPI length matching but on such relative low frequencies it doesn't matter much... Even I tried lowering QSPI clock frequency and it has no effect.