cancel
Showing results for 
Search instead for 
Did you mean: 

Setting GPIO interrupts for two identical pins

pass3master
Senior

We are developing a software application that uses GPIO interrupts.
We want to set interrupts on the same pins (PE8, PG8), but only one of them can be set to external interrupt mode in the ioc.
Is it not possible to set external interrupt mode for two different ports on the same pin?

1 ACCEPTED SOLUTION

Accepted Solutions
Karl Yamashita
Principal

Architecturally it's not possible even if you enabled them in FW. Only one will physically interrupt.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

View solution in original post

2 REPLIES 2
Karl Yamashita
Principal

Architecturally it's not possible even if you enabled them in FW. Only one will physically interrupt.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

Thank you for your reply.
We understand that this is a physical constraint, so I will close this.