cancel
Showing results for 
Search instead for 
Did you mean: 

Setting GPIO interrupts for two identical pins

pass3master
Senior

We are developing a software application that uses GPIO interrupts.
We want to set interrupts on the same pins (PE8, PG8), but only one of them can be set to external interrupt mode in the ioc.
Is it not possible to set external interrupt mode for two different ports on the same pin?

1 ACCEPTED SOLUTION

Accepted Solutions
Karl Yamashita
Lead III

Architecturally it's not possible even if you enabled them in FW. Only one will physically interrupt.

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

View solution in original post

2 REPLIES 2
Karl Yamashita
Lead III

Architecturally it's not possible even if you enabled them in FW. Only one will physically interrupt.

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

Thank you for your reply.
We understand that this is a physical constraint, so I will close this.