2008-10-17 2:47 AM
Serial Wire Debug with 2 Controllers
2011-05-17 3:48 AM
I've not seen any mention of SWD cascade in the literature. Fear the common connection of SWDIO, SWCLK seems ok. Perhaps a similar request to IAR will shed light.
Should the answer be no - believe it simplest/lowest cost to implement a SWDIO spdt switch - using a small shunt. This yields the case in which - temporarily - only one STM32 is programmed - should there be any data interconnects this may be problematic. Probably safest if you power down prior to moving the shunt from STM32 #1 to #2.2011-05-17 3:48 AM
We are designing a board with two STM32 controllers on it.
We would like to use Serial Wire Debug (SWD) interface for debugging. Is it possible to connect both controlles with one J-Link adapter (at the same time)? ->Connect SWCLK and SWDIO of both controllers together on one connector. Haven't found help on that issue in documentation. Thanks for any help.