Posted on May 17, 2011 at 13:38As described in the reference manual, the initial-value (reset) cannot be set to something else than 0xFFFFFFFF. This leads into a problem if you want to build the CRC over the whole flash memory and cannot do this wit...
Posted on May 17, 2011 at 12:48We are designing a board with two STM32 controllers on it. We would like to use Serial Wire Debug (SWD) interface for debugging. Is it possible to connect both controlles with one J-Link adapter (at the same time)? ->C...
Posted on March 30, 2009 at 11:42Hi In the technical note ''Touch sensing software library (TSSL) frequently asked and anticipated questions (FAAQs)'' it says, that the TSL is also useable on STM32 controllers. I downloaded the library for the STM8S...