cancel
Showing results for 
Search instead for 
Did you mean: 

Send 64 bytes to xbee pro S2b & send to sleep mode

aamirali641989
Associate II
Posted on June 27, 2014 at 13:07

Hi,

I need to transmit 64 bytes at a time with xbee-pro-s2b. Then send xbee into sleep since this is battery powered application.

At receiver end another xbee-pro-2b is connected which is not battery powered. So always on.

At transmitter side power is a issue, so I want to send 64 bytes at a time & then set Sleep pin high.

xbee pin will tx all the 64 bytes & go to sleep afterwards.

Is there any example code for this??

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0