cancel
Showing results for 
Search instead for 
Did you mean: 

Segger SystemView with FreeRTOS

Aquib  Fateh
Associate
Posted on September 22, 2017 at 08:50

Has anyone tried using Segger's SystemView on a FreeRTOS project. I am trying to get SystemView working on a FreeRTOS project created using CubeMX.

I am having trouble patching the FreeRTOS files with the patch file provided by Segger. 

Thanks

4 REPLIES 4
Evgeny Erlihman
Associate III
Posted on November 10, 2017 at 19:03

Any progress with this?

Joerg Wagner
Senior III
Posted on December 12, 2017 at 19:22

I did. Replace your ST-Link Firmware with SEGGER Firmware and follow the instructions in their PDF document

or use a J-Link (EDU) to achieve a better performance when you want to debug parallel.

- Joerg -

0690X00000609CKQAY.png
Posted on December 12, 2017 at 19:29

I am using a NUCLEO-H743ZI, and for some reason neither systemview nor jscope could find _SEGGER_RTT automatically, when it was located in DTCM. So i moved it to RAM_D1, and it resolved the issue...

Richard Lowe
Senior III
Posted on December 12, 2017 at 20:58

I use both SystemView and Jscope extensively. Both on a Linux host.

You'll need to match the patch with the version of FreeRTOS. V9 is current and the V9 patch is available as well.

What issues are you having in particular?

I've included my entire FreeRTOS source that has already been patched.

________________

Attachments :

FreeRTOS.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyG9&d=%2Fa%2F0X0000000b56%2FEFXyowB0WXdvyEE.qMcI7EUi6g8uV_oAeOHfLPeTzHo&asPdf=false