Solved
SDIO/EMMC version of STM32 versus EMMC IC version
Hi
I want to use an EMMC( INSIGNIS NSEC53K) with STM32F405 SDIO interface.
- STM32F405 manual says: "Full compliance wit MhultiMediaCard System Specification Version 4.2."
- the EMMCwe have chosen: INSIGNIS NSEC53K. Its datasheet says:"Compliant with eMMC Specification Ver. 4.4, 4.41, 4.5, 5.0"
Are these 2 kompatibel with each other? Will this work?
At the moment I reach transferstate, but before I spend more time on it, it would be nice to know if there will be major issues.
Which stm32 SDIO/SDMMC interfaces have a MMC spec version >= 4.4?
Thanks