Question
SD Card SDIO not working(FR_DISK_ERR)
I have a custom board and I have to run an SD card on it using SDIO protocol however on f_mount() function it takes a long time to come out with error FR_DISK_ERR but when I call "HAL_SD_GetCardInfo(&hsd, &sdCardSpace)" then I am getting all the data. I have tried with both 1-bit and 4-bit SDIO and DMA but none is working. I need help to figure out if its hardware error or software error or what the error is.