sd card init problem
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-01-02 5:28 AM
Posted on January 02, 2015 at 14:28
My STM32F429 board uses Kingston 4GB uSDHC card. CubeF4v1.3.0 HAL init fails in
SD_PowerON() function in stm32f4xx_hal_sd.c /* Send CMD55 */ sdio_cmdinitstructure.Argument = 0; sdio_cmdinitstructure.CmdIndex = SD_CMD_APP_CMD; SDIO_SendCommand(hsd->Instance, &sdio_cmdinitstructure); /* Check for error conditions */ errorstate = SD_CmdResp1Error(hsd, SD_CMD_APP_CMD); /* If errorstate is Command TimeOut, it is a MMC card */ /* If errorstate is SD_OK it is a SD card: SD card 2.0 (voltage range mismatch) or SD card 1.x */if(errorstate == SD_OK)
{ /* SD CARD */ /* Send ACMD41 SD_APP_OP_COND with Argument 0x80100000 */ while((!validvoltage) && (count < SD_MAX_VOLT_TRIAL)) { /* SEND CMD55 APP_CMD with RCA as 0 */ sdio_cmdinitstructure.Argument = 0; sdio_cmdinitstructure.CmdIndex = SD_CMD_APP_CMD; sdio_cmdinitstructure.Response = SDIO_RESPONSE_SHORT; sdio_cmdinitstructure.WaitForInterrupt = SDIO_WAIT_NO; sdio_cmdinitstructure.CPSM = SDIO_CPSM_ENABLE; SDIO_SendCommand(hsd->Instance, &sdio_cmdinitstructure); I check SD_CMD and SD_CLK with oscilloscope: 1) 400kHz clock starts, 2) CMD0 then CMD8 sent 3) 200usec no response 4) CMD55 send (payload 0) 5) response after 4 clk cycles: 0x 37 00 80 01 20 04 which is CMD55 response, CRC is x04 If I stop at the breakpoint (red line in code),errorstate variable
contains 15: SD_COM_CRC_FAILED. For me CRC 0000100 seems to be fine for that message, I don't know why ''errorstate'' fails, but init won't continue with AMCD41... I've tried it with other 8GB Kingston microSD HD...same thing. Any idea what can cause this? #sd-card-init
Labels:
- Labels:
-
SDIO-SDMMC
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-01-04 2:46 AM
Posted on January 04, 2015 at 11:46
To be exact, response sent by the SD card is 0x 37 00 80 01 20
09
, where last byte is 0000100 7-bit CRC and ''1'' stop bit. I calculated CRC by online calculator:https://ghsi.de/CRC/index.php?Polynom=10001001&Message=37+00+80+01+20
Polynom is x7 + x3 + x0 for calculation.