2014-04-23 5:39 AM
When you enable any part in the ADC (F401RET 64pin mcu) you get a java-crash:
Apr 23, 2014 2:03:11 PM com.st.microxplorer.util.LogicalParser checkConditionSEVERE: nullcom.bestcode.mathparser.ParserException: ExpNtVld at com.bestcode.mathparser.MathParserImpl.createParseTree(MathParserImpl.java:801) at com.bestcode.mathparser.MathParserImpl.createParseTree(MathParserImpl.java:797) at com.bestcode.mathparser.MathParserImpl.createParseTree(MathParserImpl.java:800) at com.bestcode.mathparser.MathParserImpl.parse(MathParserImpl.java:411) at com.bestcode.mathparser.MathParserImpl.evaluate(MathParserImpl.java:323) at com.bestcode.mathparser.MathParserImpl.getValue(MathParserImpl.java:255) at com.st.microxplorer.util.LogicalParser.evaluate(LogicalParser.java:234) at com.st.microxplorer.util.LogicalParser.checkCondition(LogicalParser.java:187)...
(both on m$ and linux platforms)Does the crash have any impact ? or is just usual sloppy java-programmer style ?Many regardsLars OlePS! Why are the - almost perfectly normal - java code wrapped in m$-selfextracting .exe files ?PPS! Running the javacode on standalone linux works almost 100% - except when trying to configure GPIO-pins:fitInWindow Computed Zoom: 0.8InternalPropertyChange: setIPParameter OLD value:RCC / NEW value:Never MindInternalPropertyChange: changePin GPIO_OutputException in thread ''AWT-EventQueue-0'' java.lang.NullPointerException at com.st.microxplorer.plugins.ip.gpio.gui.ParameterUI.addPropertyChangeListener(ParameterUI.java:157) at javax.swing.plaf.synth.SynthPanelUI.installListeners(Unknown Source) at javax.swing.plaf.synth.SynthPanelUI.installUI(Unknown Source) at javax.swing.JComponent.setUI(Unknown Source) at javax.swing.JPanel.setUI(Unknown Source) at javax.swing.JPanel.updateUI(Unknown Source) at javax.swing.JPanel.<init>(Unknown Source) at javax.swing.JPanel.<init>(Unknown Source) at javax.swing.JPanel.<init>(Unknown Source) at com.st.microxplorer.plugins.ip.gpio.gui.ParameterUI.<init>(ParameterUI.java:68) at com.st.microxplorer.plugins.ip.gpio.gui.ParameterUI.<init>(ParameterUI.java:95) #java-crash2014-04-24 1:54 AM
STM32CubeMX is not yet supported on Linux.
2014-04-27 10:06 AM
Seems though as you're very close to a linux solution ;)
I'll gladly give some help ?!RegardsLars Ole