2023-08-11 10:22 AM
Hello all.
I have troubles porting SBSFU onto STM32F756ZGTx.
I took 1 image sample for STM32F769I as a base. I modified:
- STM32F756ZGTx_FLASH.ld (SECoreBin)
- STM32F756ZGTx_FLASH.ld (SBSFU)
- mapping_sbsfu.ld
- mapping_fwimg.ld
- Other changes to source code under SBSFU and SECoreBin to work with target platform.
Unfortunately, it still doesn't work and I'm not able to find out why.
I connected debugger and every time programs ends up in a hard fault handler...
With SFU_MPU_PROTECT_ENABLE turned off:
With SFU_MPU_PROTECT_ENABLE turned on:
First debugger starts here
Then it fails upon calling SFU_BOOT_SystemSecurity_Config() -> SFU_COM_Init() -> setvbuf():
If necessary I can provide snippets of code. Thanks!
Solved! Go to Solution.
2023-08-16 05:10 AM
Problem solved. Issue came from missing line inside SBSFU linker script. So next time I should be more focused 🙂
PS. It doesn't mean that tool or naming is fine. Build analyzer shouldn't show misleading information.
2023-08-12 08:02 PM
I don't know if it can help in your case, but I found these videos about advanced debugging:
[STM32CubeIDE Advanced Debug Features]
Complement for some models:
2023-08-14 09:33 AM
Thanks! I didn't solve the issue but did help finding this out:
That's the information from built in build analyzer for SBSFU.elf. I have no clue why SE_Entry_Secure_ROM_Region is that huge occupying 3729% of allocated memory.
2023-08-14 09:44 AM
3729%
Went a little over the top 😅
2023-08-14 09:47 AM
Just a little bit :D
I would like to know why since we are stuck on it for a long time. I saw similar thread on that forum but nobody replied to it.
2023-08-14 09:47 AM
There are some videos about SBSFU on YouTube:
https://www.youtube.com/@stmicroelectronics/search?query=SBSFU
2023-08-14 09:48 AM
Yeah, I know. But doesn't help too much. Maybe I have to watch them again and find that missing piece. I hoped that someone experienced something similar and knows how to deal with it.
2023-08-15 04:07 AM - edited 2023-08-15 04:15 AM
Okay, so that's weird, but I built two different sample projects:
Both presents same misleading information that there is some issue with memory mapping. The thing is that NUCLEO-L432KC works totally fine. Looks like it's not an issue with the build itself, but with the tool or naming used throughout linker files. Correct me if I'm wrong.
2023-08-16 05:10 AM
Problem solved. Issue came from missing line inside SBSFU linker script. So next time I should be more focused 🙂
PS. It doesn't mean that tool or naming is fine. Build analyzer shouldn't show misleading information.