2024-12-29 11:18 PM - edited 2024-12-29 11:43 PM
Hi
I want to understand Rx message process in case of can2. Rx fifo code I have tested when I used only CAN1 it is working fine. I have put RxFifoMSgpendingcallback function in IRQhandler and further code is working fine for when I used only one (CAN1) controller ,can you help me to understand what change I should do when I am using CAN1 and CAN2 both controller so that I can receive for both controller data.
/* Receive FIFO 0 message pending interrupt management *********************/
if ((interrupts & CAN_IT_RX_FIFO0_MSG_PENDING) != 0U)
{
/* Check if message is still pending */
if ((hcan->Instance->RF0R & CAN_RF0R_FMP0) != 0U)
{
/* Receive FIFO 0 message pending Callback */
#if USE_HAL_CAN_REGISTER_CALLBACKS == 1
/* Call registered callback*/
hcan->RxFifo0MsgPendingCallback(hcan);
#else
/* Call weak (surcharged) callback */
HAL_CAN_RxFifo0MsgPendingCallback(hcan);
#endif /* USE_HAL_CAN_REGISTER_CALLBACKS */
}
}
void CANRxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
CAN_RxHeaderTypeDef rx_header;
uint8_t rx_data[8];
if (HAL_CAN_GetRxMessage(&hcan1, CAN_RX_FIFO0, &rx_header, rx_data) != HAL_OK)
{
Error_Handler();
}
}
HAL_StatusTypeDef HAL_CAN_GetRxMessage(CAN_HandleTypeDef *hcan, uint32_t RxFifo,
CAN_RxHeaderTypeDef *pHeader, uint8_t aData[])
{
HAL_CAN_StateTypeDef state = hcan->State;
assert_param(IS_CAN_RX_FIFO(RxFifo));
if ((state == HAL_CAN_STATE_READY) ||
(state == HAL_CAN_STATE_LISTENING))
{
/* Check the Rx FIFO */
if (RxFifo == CAN_RX_FIFO0) /* Rx element is assigned to Rx FIFO 0 */
{
/* Check that the Rx FIFO 0 is not empty */
if ((hcan->Instance->RF0R & CAN_RF0R_FMP0) == 0U)
{
/* Update error code */
hcan->ErrorCode |= HAL_CAN_ERROR_PARAM;
return HAL_ERROR;
}
}
else /* Rx element is assigned to Rx FIFO 1 */
{
/* Check that the Rx FIFO 1 is not empty */
if ((hcan->Instance->RF1R & CAN_RF1R_FMP1) == 0U)
{
/* Update error code */
hcan->ErrorCode |= HAL_CAN_ERROR_PARAM;
return HAL_ERROR;
}
}
/* Get the header */
pHeader->IDE = CAN_RI0R_IDE & hcan->Instance->sFIFOMailBox[RxFifo].RIR;
if (pHeader->IDE == CAN_ID_STD)
{
pHeader->StdId = (CAN_RI0R_STID & hcan->Instance->sFIFOMailBox[RxFifo].RIR) >> CAN_TI0R_STID_Pos;
}
else
{
pHeader->ExtId = ((CAN_RI0R_EXID | CAN_RI0R_STID) &
hcan->Instance->sFIFOMailBox[RxFifo].RIR) >> CAN_RI0R_EXID_Pos;
}
pHeader->RTR = (CAN_RI0R_RTR & hcan->Instance->sFIFOMailBox[RxFifo].RIR);
if (((CAN_RDT0R_DLC & hcan->Instance->sFIFOMailBox[RxFifo].RDTR) >> CAN_RDT0R_DLC_Pos) >= 8U)
{
/* Truncate DLC to 8 if received field is over range */
pHeader->DLC = 8U;
}
else
{
pHeader->DLC = (CAN_RDT0R_DLC & hcan->Instance->sFIFOMailBox[RxFifo].RDTR) >> CAN_RDT0R_DLC_Pos;
}
pHeader->FilterMatchIndex = (CAN_RDT0R_FMI & hcan->Instance->sFIFOMailBox[RxFifo].RDTR) >> CAN_RDT0R_FMI_Pos;
pHeader->Timestamp = (CAN_RDT0R_TIME & hcan->Instance->sFIFOMailBox[RxFifo].RDTR) >> CAN_RDT0R_TIME_Pos;
/* Get the data */
aData[0] = (uint8_t)((CAN_RDL0R_DATA0 & hcan->Instance->sFIFOMailBox[RxFifo].RDLR) >> CAN_RDL0R_DATA0_Pos);
aData[1] = (uint8_t)((CAN_RDL0R_DATA1 & hcan->Instance->sFIFOMailBox[RxFifo].RDLR) >> CAN_RDL0R_DATA1_Pos);
aData[2] = (uint8_t)((CAN_RDL0R_DATA2 & hcan->Instance->sFIFOMailBox[RxFifo].RDLR) >> CAN_RDL0R_DATA2_Pos);
aData[3] = (uint8_t)((CAN_RDL0R_DATA3 & hcan->Instance->sFIFOMailBox[RxFifo].RDLR) >> CAN_RDL0R_DATA3_Pos);
aData[4] = (uint8_t)((CAN_RDH0R_DATA4 & hcan->Instance->sFIFOMailBox[RxFifo].RDHR) >> CAN_RDH0R_DATA4_Pos);
aData[5] = (uint8_t)((CAN_RDH0R_DATA5 & hcan->Instance->sFIFOMailBox[RxFifo].RDHR) >> CAN_RDH0R_DATA5_Pos);
aData[6] = (uint8_t)((CAN_RDH0R_DATA6 & hcan->Instance->sFIFOMailBox[RxFifo].RDHR) >> CAN_RDH0R_DATA6_Pos);
aData[7] = (uint8_t)((CAN_RDH0R_DATA7 & hcan->Instance->sFIFOMailBox[RxFifo].RDHR) >> CAN_RDH0R_DATA7_Pos);
/* Release the FIFO */
if (RxFifo == CAN_RX_FIFO0) /* Rx element is assigned to Rx FIFO 0 */
{
/* Release RX FIFO 0 */
SET_BIT(hcan->Instance->RF0R, CAN_RF0R_RFOM0);
}
else /* Rx element is assigned to Rx FIFO 1 */
{
/* Release RX FIFO 1 */
SET_BIT(hcan->Instance->RF1R, CAN_RF1R_RFOM1);
}
/* Return function status */
return HAL_OK;
}
else
{
/* Update error code */
hcan->ErrorCode |= HAL_CAN_ERROR_NOT_INITIALIZED;
return HAL_ERROR;
}
}