cancel
Showing results for 
Search instead for 
Did you mean: 

Running application in "Release mode causes errors"

HNall.1
Associate III

Hi all,

I'm trying to profile my application which running on STM32F469IH6 micro-controller.

I'm able to run the application in debug mode and able to see the timings of the applications.

But In generally running application in release mode will have more optimizations included compared with the debug mode. But If I run the application in Release mode then i'm encountered with below error.0693W000003PSBYQA4.png

Below is log at the time of running application in release mode:

STMicroelectronics ST-LINK GDB server. Version 5.6.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
 
Starting server with the following options:
        Persistent Mode            : Disabled
        Logging Level              : 1
        Listen Port Number         : 61234
        Status Refresh Delay       : 15s
        Verbose Mode               : Disabled
        SWD Debug                  : Enabled
        InitWhile                  : Enabled
 
Waiting for debugger connection...
Debugger connected
      -------------------------------------------------------------------
                       STM32CubeProgrammer v2.5.0-RC1                  
      -------------------------------------------------------------------
 
ST-LINK SN  : 066DFF535254887767171939
ST-LINK FW  : V2J37M26
Board       : 32F469IDISCOVERY
Voltage     : 3.27V
SWD freq    : 4000 KHz
Connect mode: Under Reset
Reset mode  : Hardware reset
Device ID   : 0x434
Revision ID : Rev A
Device name : STM32F469xx/F467xx
Flash size  : 2 MBytes
Device type : MCU
Device CPU  : Cortex-M4
 
 
 
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a09660.srec
  File          : ST-LINK_GDB_server_a09660.srec
  Size          : 676208 Bytes
  Address       : 0x08000000 
 
 
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 9]
Download in Progress:
 
 
File download complete
Time elapsed during download operation: 00:00:12.201
 
 
 
Verifying ...
 
 
 
 
Download verified successfully 
 
 
Debugger connection lost.
Shutting down...
 

Thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
20 REPLIES 20
PHill.1
Associate

Most of the STM32 MCUS have in place execution, that is instructions are executed directly from flash, so you typically dont loade the whole application into memory.