cancel
Showing results for 
Search instead for 
Did you mean: 

STM32N6570-DK: Break at address 0x18003A1A with no debug information when running CubeMX-generated project

MownishBugatha
Associate II

MownishBugatha_0-1770187275194.png

I generated a project using STM32CubeMX for the STM32N6570-DK board.

Steps performed:

  1. Generated code using CubeMX (default configuration)

  2. Imported project into STM32CubeIDE

  3. Built the project successfully (no build errors)

  4. Attempted to run/debug the application

During programming / start of execution, the debugger stops with the following message:

Break at address “0x18003A1A” with no debug information available, or outside of program code

0 REPLIES 0