cancel
Showing results for 
Search instead for 
Did you mean: 

RUN_PD bit not found in RM0503

KSB
Associate II

 

As shown in the screenshot below. RUN_PD bit is mentioned here and nowhere else in the entire Reference manual.

 

KSB_1-1725335379036.png

 

2 REPLIES 2
STTwo-32
ST Employee

Hello @KSB 

Thank you so much for reporting this issue. I've escalated to the concerned team for correction on the coming release of the document (under internal ticket number 190285).

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello @STTwo-32,

When will RM0503 be updated to clarify support for a RUN_PD bit? Can you at least confirm if this functionality is supported? I am prototyping a project now that may depend on this feature.

Regards,
Clyne