cancel
Showing results for 
Search instead for 
Did you mean: 

RTC Wakeup timer stops generating interrupt.

KNath.1
Associate

Hello,

I am using RTC Wakeup timer in STM32F469NIH6 processor. Low level access is using HAL code.

I's is configured with

RTC.CR.WCKSEL = 0x3

RTC.WTR.WUT = 1

EXTI.IMR.MR22 is set

EXTI.RSTR.M22 is set.

It generates RTC Wakeup Interrupt ~122.09usec. interval for about .8sec. After that no more interrupt.

RTC.ISR.WUTF is set

EXTI.PR.M22 is not set

What could be the reason for not generating interrupt any more.

Thanks.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0