2012-12-22 10:12 AM
Hi,
I just added backup battery to the F407 discovery board. All seem to work ok, the RTC counts while the CPU is on and in Stop mode as well. But if i remove the power all together the last RTC value is preserved by the battery, but no update on the RTC is done. Reading the pdf few times and all possible posts on the forum, i am more confused. Maybe my RTC init is bad ? RTC_InitTypeDef RTC_InitStructure; RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE); // Allow access to BKP Domain PWR_BackupAccessCmd(ENABLE); #ifdef RTC_CLOCK_SOURCE_LSI // Enable the LSI OSC RCC_LSICmd(ENABLE); // Wait till LSI is ready while(RCC_GetFlagStatus(RCC_FLAG_LSIRDY) == RESET); // Select the RTC Clock Source RCC_RTCCLKConfig(RCC_RTCCLKSource_LSI); RTC_InitStructure.RTC_AsynchPrediv = 0x7F; RTC_InitStructure.RTC_SynchPrediv = 0xFF; #endif #ifdef RTC_CLOCK_SOURCE_LSE // Enable the LSE OSC RCC_LSEConfig(RCC_LSE_ON); // Wait till LSR is ready while(RCC_GetFlagStatus(RCC_FLAG_LSERDY) == RESET); // Select the RTC Clock Source RCC_RTCCLKConfig(RCC_RTCCLKSource_LSE); RTC_InitStructure.RTC_AsynchPrediv = 0x7F; RTC_InitStructure.RTC_SynchPrediv = 0xFF; #endif // Enable the RTC Clock RCC_RTCCLKCmd(ENABLE); // Wait for RTC APB registers synchronisation (needed after start-up from Reset) RTC_WaitForSynchro(); // Set the RTC time base to 1s RTC_InitStructure.RTC_HourFormat = RTC_HourFormat_24; if (RTC_Init(&RTC_InitStructure) == ERROR) { // User can add here some code to deal with this error //while(1); } // Enable BKPRAM Clock //RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_BKPSRAM, ENABLE); // Enable the Backup SRAM low power Regulator //PWR_BackupRegulatorCmd(ENABLE); // Wait until the Backup SRAM low power Regulator is ready //while(PWR_GetFlagStatus(PWR_FLAG_BRR) == RESET); I am on LSI clock right now. Regards, Chris2012-12-22 3:06 PM
I am on LSI clock right now.
Well that's your problem right there, the battery only runs the LSE as it uses a lot less power.
2012-12-22 3:13 PM
RM0090
4.1.2 Battery backup domainBackup domain description
To retain the content of the RTC backup registers, backup SRAM, and supply the RTC when VDD is turned off, VBAT pin can be connected to an optional standby voltage supplied by a battery or by another source.
To allow the RTC to operate even when the main digital supply (VDD) is turned off, the VBAT pin powers the following blocks:
�? The RTC
�? The LSE oscillator
�? The backup SRAM when the low power backup regulator is enabled
�? PC13 to PC15 I/Os, plus PI8 I/O (when available)
The switch to the VBAT supply is controlled by the power-down reset embedded in the Reset block.
2012-12-23 2:52 AM
Thanks clive,
My bad again, reading but not comprehending. And i didn't test because the oscillator i bought will not start (12.5pF loading capacitance), but read too late about the limitation. One final question on the subject. Do you think is ok to run the RTC on HSE clock during normal operation, to minimize the noise floor, but before going to stop mode switch to LSE ? This clock switching will maybe make the clock to loose sync for a while and loose precision ? Also in this case i will still have the surprise power removal problem i guess. BR, Chris Update: All works now, it seems i have bought the 6pF version of the oscillator, but the two extra capacitors values are very critical - 6.8pF were no go, extra 1pF in parallel made it work (8pF required by the pdf).