cancel
Showing results for 
Search instead for 
Did you mean: 

RM0091 - is FLASH prefetch after reset on or off?

waclawek.jan
Super User

In RM0091, rev.9, 3.5.1 Flash access control register (FLASH_ACR):

Reset value: 0x0000 0000

[...]

Bit 4 PRFTBE: Prefetch buffer enable

 0: Prefetch is disabled

In RM0091, rev.9, Prefetch controller  within 3.2.1:

After reset, the state of the prefetch buffer is on.

ST, please clarify.

JW

(https://community.st.com/s/question/0D50X00009XkaBB/stm32f0xx-findings last post)

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee

Hello @Community member​ ,

Thanks for your post.

I will check this and take the necessary action.

Edit: you can enable Prefetch at startup, very low consumption impact and software overhead for granted improve performance, except if you run at 24MHz max freq.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
waclawek.jan
Super User

Thanks, Imen.

Jan