2021-03-22 1:18 PM
Hello,
I recently upgraded to CubeIde 1.6.0 but I am having many new problems when programming STM32h/43: the configurations generation is much slower and it often stops updating all needed files, which forces me to reboot (I could not find a better way).
So I decided to downgrade to 1.5.1 which was stable for me, but I cannot load the .ioc files that were generated with 1.6.0. Is there a workaround?
Solved! Go to Solution.
2023-05-04 11:50 AM
Open the IOC file in a text editor and change the line "MxCube.Version=***" to the version of CubeMX that your version of the IDE wants you to have.
2021-03-22 1:59 PM
>>Is there a workaround?
I'm sensing there isn't, I guess you could try a text editor or a merge tool to understand the change in features/structure.
Importing older .IOC has been a challenge at times, I'd definitely recommend doing this into a sandbox project rather than a live one, as file loss has been reported on multiple occasions.
2023-05-04 11:50 AM
Open the IOC file in a text editor and change the line "MxCube.Version=***" to the version of CubeMX that your version of the IDE wants you to have.
2023-10-09 10:18 PM
wow, it really works for opening the 6.3.0 version ioc file by cubemx 6.2.0, thanks bro
2024-02-05 11:19 PM
Yes it work but MxCube.Version=**** we need to set MxDb.Version=**** acordinglly.
Thankyou so much your advice is very helpful.