2024-06-04 02:02 AM
Hi all,
I have working on USBPD Sink project in that ,I have been struck in the part of reading the voltage from the STM32L562CET6(Customized Board)before this process I have done the same project in STM32L562E-DK , What I need to do actually to overcome the issue of mine?
2024-11-16 10:19 PM
To overcome the issue, ensure the ADC configuration on your customized STM32L562CET6 board matches the setup from the STM32L562E-DK. Verify that the voltage sensing pin and associated circuitry are correctly connected and aligned with the reference design. Additionally, check the firmware to confirm proper initialization of ADC and USBPD settings specific to your custom board.