2025-01-21 10:14 PM
Configured the controller stm32l151c8t6a to work in low power run mode ( UART peripheral running) but the current consumption is going upto 6.2mA. After disabling the uart peripheral the consumption decreases upto 4.2mA. In real situation we are going to use SPI,DAC,ADC and UART so in reality the consumption will not decrease but increase. So is there any way of decreasing the current consumption upto 3.8mA?
2025-01-24 06:00 AM - edited 2025-01-24 08:24 AM
Hello @PratikMore and welcome to the community;
are the free pins configured as analog? Could you try to set all free pins as analog to optimize the power consumption.
I recommend you look at these FAQs and example may help you to optimize the power consumption.
I hope this help you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-24 09:15 AM
Look at what's attached to the pins, that's often where the current consumption is coming from, as the STM has to sink/source what the external circuit draws.
If going to RS232 level shifters, perhaps look at ones with a signal indicating external connectivity, and able to gate supply.
2025-01-24 10:34 AM
You some miss. Real MCU current can be very low as you see in table
and combined with STOP under 600nA.