2012-08-31 11:51 AM
Hi,
at the moment I'm using the following code to recieve a byte:char
ReceivedData = NULL;
void
main() {
.
.
.
while
(1){
/* Wait until a byte is received */
while
(USART_GetFlagStatus(USART2, USART_FLAG_RXNE) == RESET)
{
}
/* read byte and print via usart2 it */
ReceivedData = USART_ReceiveData(USART2);
printf
(
''Positionen: %d \r\n''
, ReceivedData);
//abbort if 3 received
if
(ReceivedData == 3)
break
;
}
.
.
}
I now want to recieve more then 1 byte and store it an recieve Buffer ''RXBUFF[]''.
Because I want to send a byte array from my pc to the controller and then I want to deserialze the data to int16 or int32 ...
How can i achieve that?
how can I recieve my bytearray with the stm32f103 ?
WR
Alex
#usart-stm32-loopback #usart-stm32
2012-09-02 5:15 AM
I'd probably do some of the processing under interrupt, and make some effort to validate and synchronize the incoming data.
As to books, I learned C and Assembler a very long time ago. The K&R book is the best reference for C. For the Cortex-M3, you could start with the ARM Technical Manuals, and Joseph Yiu's fine books, anyone of his Cortex series/editions would provide a good grounding. The STM32 specific stuff is covered well in the Data Sheets and Reference Manuals. I suspect however you're looking for something that covers more of the mechanics of how things work in general. In this regard I'd suggest looking at some of the microprocessor books of the early 80's, while they didn't consider themselves ''embedded'' back then at lot of the systems are similar and resource limited, and addressed a lot of fundamental issues.2014-06-14 7:26 AM
Hi all,
I have the same problem using interrupts with UART. Why handler is called once if I have sent 20 bytes from my PC? Should it be called every byte is in buffer? here is the handler and initUart code:// this is the interrupt request handler (IRQ) for ALL USART1 interruptsvoid USART1_IRQHandler(void){ static uint8_t cnt = 0; // this counter is used to determine the string length //Data available in the Read Register. if( USART_GetITStatus(USART1, USART_IT_RXNE) != RESET ) { RXBUFF[cnt++] = USART_ReceiveData(USART1); // the character from the USART1 data register is saved in t } if(MAX_STRLEN > cnt) { cnt = 0; }}and here is init of UARTvoid initUSART1(uint32_t baudrate){ GPIO_InitTypeDef GPIO_InitStruct; // this is for the GPIO pins used as TX and RX USART_InitTypeDef USART_InitStruct; // this is for the USART1 initilization NVIC_InitTypeDef NVIC_InitStructure; // this is used to configure the NVIC (nested vector interrupt controller) /* enable APB2 peripheral clock for USART1 * note that only USART1 and USART6 are connected to APB2 * the other USARTs are connected to APB1 */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); /* enable the peripheral clock for the pins used by * USART1, PB6 for TX and PB7 for RX */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); /* This sequence sets up the TX and RX pins * so they work correctly with the USART1 peripheral */ GPIO_InitStruct.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7; // Pins 6 (TX) and 7 (RX) are used GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF; // the pins are configured as alternate function so the USART peripheral has access to them GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz; // this defines the IO speed and has nothing to do with the baudrate! GPIO_InitStruct.GPIO_OType = GPIO_OType_PP; // this defines the output type as push pull mode (as opposed to open drain) GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP; // this activates the pullup resistors on the IO pins GPIO_Init(GPIOB, &GPIO_InitStruct); // now all the values are passed to the GPIO_Init() function which sets the GPIO registers /* The RX and TX pins are now connected to their AF * so that the USART1 can take over control of the * pins */ GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_AF_USART1 ); GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_AF_USART1 ); /* Now the USART_InitStruct is used to define the * properties of USART1 */ USART_InitStruct.USART_BaudRate = baudrate; // the baudrate is set to the value we passed into this init function USART_InitStruct.USART_WordLength = USART_WordLength_8b; // we want the data frame size to be 8 bits (standard) USART_InitStruct.USART_StopBits = USART_StopBits_1; // we want 1 stop bit (standard) USART_InitStruct.USART_Parity = USART_Parity_No; // we don't want a parity bit (standard) USART_InitStruct.USART_HardwareFlowControl = USART_HardwareFlowControl_None; // we don't want flow control (standard) USART_InitStruct.USART_Mode = USART_Mode_Tx | USART_Mode_Rx; // we want to enable the transmitter and the receiver USART_Init(USART1, &USART_InitStruct); // again all the properties are passed to the USART_Init function which takes care of all the bit setting /* Here the USART1 receive interrupt is enabled * and the interrupt controller is configured * to jump to the USART1_IRQHandler() function * if the USART1 receive interrupt occurs */ USART_ITConfig(USART1, USART_IT_RXNE, ENABLE); // enable the USART1 receive interrupt NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn; // we want to configure the USART1 interrupts NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; // this sets the priority group of the USART1 interrupts NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; // this sets the subpriority inside the group NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; // the USART1 interrupts are globally enabled NVIC_Init(&NVIC_InitStructure); // the properties are passed to the NVIC_Init function which takes care of the low level stuff // finally this enables the complete USART1 peripheral USART_Cmd(USART1, ENABLE);}2014-06-14 8:05 AM
Why handler is called once if I have sent 20 bytes from my PC?
Because at 9600 baud, one character takes ~1ms to arrive, so figure several hundred thousand processor cycles, you interrupt so the processor can do useful work while the signal is on the wire, and it's one byte because of the silicon/power resources needed to provide larger buffers.2014-06-14 8:34 AM
I can use baud 57600. I suppose to send single bytes in a eg. loop from the sender module? I am creating a BT app on android which is a sender.
2014-06-14 9:38 AM
I can use baud 57600. I suppose to send single bytes in a eg. loop from the sender module? I am creating a BT app on android which is a sender.
You can send and transmit continuous streams of characters, they do however arrive/depart periodically depending on the transmission rate, so dozens of characters aren't all going to arrive at once. One typically handles this by buffering the data, and managing the transmission/reception in an interrupt. You don't mention a part/board, I'll assume for my convenience that you have an STM32F4-Discovery board.[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/STM32F4%20problem%20with%20USART1%20INTERRUPT&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=553]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32Discovery%2FSTM32F4%20problem%20with%20USART1%20INTERRUPT&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=553[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/STM32F4%20problem%20with%20USART1%20INTERRUPT&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=553]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32Discovery%2FSTM32F4%20problem%20with%20USART1%20INTERRUPT&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=553[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/UART%20example%20code%20for%20STM32F0&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=12897]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32Discovery%2FUART%20example%20code%20for%20STM32F0&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=128972014-06-14 10:03 AM
if(MAX_STRLEN > cnt)
{
cnt = 0;
}
This looks suspicious, cnt is lower than max length and reset every time.
2014-06-15 11:36 PM
2014-08-07 8:05 AM
while
(1)
{
while
(USART_GetFlagStatus(USART1, USART_FLAG_RXNE) == RESET);
RXBUFF[j] = USART_ReceiveData(USART1);
if
(USART_GetFlagStatus(USART1, USART_FLAG_TXE) != RESET)
USART_SendData(USART1, RXBUFF[j]);
j++;
if
(j >= 248)
j = 0;
}
}
I have written this code, and now, I am receiving data from GPS on USART1 and now I just want to display it on the LCD.
How can I do this without transmitting it anywhere?
I can display strings on LCD too. I have written a function for that.
Please help as to where can I place that function call??
2014-08-07 9:35 AM
Really no idea what board or STM32 you're using.
For GPS NMEA stream, you might want to look at the line buffering example, and send the string to the display after the string is NUL terminated.[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/UART%20example%20code%20for%20STM32F0&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=12897]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/UART%20example%20code%20for%20STM32F0&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=128972014-08-07 10:46 PM
unsigned
char
value,i,lati_value[15],lati_dir, longi_value[15], longi_dir,
time
[10], speed[10], date[6];
unsigned
char
usart_getch()
{
/* Wait until the data is ready to be received. */
while
((USART1->ISR & USART_ISR_RXNE) == RESET){
}
return
USART1->RDR;
}
void
readgps()
{
int
q;
value=usart_getch();
if
(value==
'$'
)
{
value=usart_getch();
if
(value==
'G'
)
{
value=usart_getch();
if
(value==
'P'
)
{
value=usart_getch();
if
(value==
'R'
)
{
value=usart_getch();
if
(value==
'M'
)
{
value=usart_getch();
if
(value==
'C'
)
{
value=usart_getch();
if
(value==
','
)
{
time
[0]=usart_getch();
value=
time
[0];
for
(q=1;q<6;q++)
{
time
[q]=usart_getch();
value=
time
[q];
}
value=usart_getch();
while
(value!=
','
)
{
value=usart_getch();
}
value=usart_getch();
while
(value!=
','
)
{
value=usart_getch();
}
lati_value[0]=usart_getch();
value=lati_value[0];
for
(i=1;i<9;i++)
{
lati_value[i]=usart_getch();
value=lati_value[i];
}
while
(value!=
','
)
{
value=usart_getch();
}
lati_dir=usart_getch();
value=usart_getch();
while
(value!=
','
)
{
value=usart_getch();
}
longi_value[0]=usart_getch();
value=longi_value[0];
for
(i=1;i<10;i++)
{
longi_value[i]=usart_getch();
value=longi_value[i];
}
while
(value!=
','
)
{
value=usart_getch();
}
longi_dir=usart_getch();
value=usart_getch();
while
(value!=
','
)
{
value=usart_getch();
}
i=0;
value=usart_getch();
while
(value!=
','
)
{
speed[i]= value;
value=usart_getch();
i++;
}
value=usart_getch();
while
(value!=
','
)
{
value=usart_getch();
}
i=0;
while
(i<6)
{
date[i]=usart_getch();
i++;
}
}
}
}
}
}
}
}