REAL TIME CLOCK (RTC)
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-27 9:33 PM
Posted on May 28, 2014 at 06:33
hello everyone
today I try to use RTC in stm32f4 cube library and some errors occur. So now I will show my code for all of you see: void dtime_bsp_open (const dtime_time_format_t fmt) { /* Configure the RTC peripheral */ g_h_rtc.Instance = RTC; if (fmt == DTIME_FORMAT_12H) { g_h_rtc.Init.HourFormat = RTC_HOURFORMAT_12; } else { g_h_rtc.Init.HourFormat = RTC_HOURFORMAT_24; } g_h_rtc.Init.AsynchPrediv = 0x007F; // datasheet rm_0090_stm32f4 22.3.9 page 544 g_h_rtc.Init.SynchPrediv = 0x00FF; // 22.6.5 page 559 g_h_rtc.Init.OutPut = RTC_OUTPUT_DISABLE; g_h_rtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH ; g_h_rtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN; /*Initialization*/if (HAL_RTC_Init(&g_h_rtc)!= HAL_OK)
{ while(1); } } and program was loop in red part. Can anyones help me about my configure is wrong?? #lse
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-29 1:29 AM
Posted on May 29, 2014 at 10:29
I reply but I don't know the cube library
With this init code RTC work on my F407 device////////////////////////////////////////////////////////////////////////////////////////////////////////////
static void RTC_RCC_config()
{
/* Enable the LSE OSC */
RCC_LSEConfig(RCC_LSE_ON);
/* Wait till LSE is ready */
while(RCC_GetFlagStatus(RCC_FLAG_LSERDY) == RESET) ;
/* Select the RTC Clock Source */
RCC_RTCCLKConfig(RCC_RTCCLKSource_LSE);
/* Enable the RTC Clock */
RCC_RTCCLKCmd(ENABLE);
}
////////////////////////////////////////////////////////////////////////////////////////////////////////////
void RTC_Drv_Init()
{
/* Allow access to RTC */
PWR_BackupAccessCmd(ENABLE);
RTC_RCC_config() ;
RTC_InitTypeDef RTC_InitStructure;
RTC_DateTypeDef RTC_DateStructure;
RTC_TimeTypeDef RTC_TimeStructure;
if (RTC_ReadBackupRegister(RTC_BKP_DR0) != RTC_BACKUP_ID)
{
/* Wait for RTC APB registers synchronisation */
RTC_WaitForSynchro();
/* Configure the RTC data register and RTC prescaler */
RTC_InitStructure.RTC_AsynchPrediv = 0x7F;
RTC_InitStructure.RTC_SynchPrediv = 0xFF;
RTC_InitStructure.RTC_HourFormat = RTC_HourFormat_24;
RTC_Init(&RTC_InitStructure);
RTC_DateStructure.RTC_Year = RTC_CFG_YROFFS;
RTC_DateStructure.RTC_Month = RTC_CFG_MONTH+1 ;
RTC_DateStructure.RTC_Date = RTC_CFG_DAY ;
RTC_DateStructure.RTC_WeekDay = RTC_CFG_DAYOFW;
RTC_SetDate(RTC_Format_BIN, &RTC_DateStructure);
RTC_TimeStructure.RTC_H12 = RTC_H12_AM;
RTC_TimeStructure.RTC_Hours = RTC_CFG_HOUR;
RTC_TimeStructure.RTC_Minutes = RTC_CFG_MIN ;
RTC_TimeStructure.RTC_Seconds = RTC_CFG_SEC ;
RTC_SetTime(RTC_Format_BIN, &RTC_TimeStructure);
/* Indicator for the RTC configuration */
RTC_WriteBackupRegister(RTC_BKP_DR0, RTC_BACKUP_ID);
}
else
{
RTC_hw_read (&RTC_DateStructure, &RTC_TimeStructure) ;
}
}
static void RTC_hw_read (RTC_DateTypeDef* ldate, RTC_TimeTypeDef* ltime)
{
RTC_GetTime(RTC_Format_BIN, ltime);
RTC_GetDate(RTC_Format_BIN, ldate);
}
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-29 6:57 AM
Posted on May 29, 2014 at 15:57
I don't use the cube library but the obvious question is if your LSE oscillator works. My guess is your program hangs trying to start the LSE. Are the caps correctly matched to the crystal? ST has an app note on how to configure crystal oscillators for STM32.
Jack Peacock