2018-06-28 9:34 AM
STM32H743
To improve the accuracy of the temperature sensor measurement, each device is individually factory-calibrated by ST. The temperature sensor factory calibration data are stored by ST in the System memory area, which is accessible in Read-only mode
Please could someone point me at where I can find information on how to read the calibration parameters. Can't see anything in the device manual, the H7 reference manual or the HAL manual but probably missed it.
Solved! Go to Solution.
2018-06-28 10:04 AM
Hello Peter,
Please refer to the
https://www.st.com/resource/en/datasheet/stm32h743bi.pdf
.The memory addresses for temperature sensor raw data acquired values, at VDDA= 3.3V , 30°C and 110°C , are provided in table 90 ' Temperature sensor calibration values'.
Khouloud.
2018-06-28 9:57 AM
You dont mention which chip you're using but check section 6 of your data sheet for a table 'Temperature sensor calibration values' and it shows the register location and values
2018-06-28 10:04 AM
Hello Peter,
Please refer to the
https://www.st.com/resource/en/datasheet/stm32h743bi.pdf
.The memory addresses for temperature sensor raw data acquired values, at VDDA= 3.3V , 30°C and 110°C , are provided in table 90 ' Temperature sensor calibration values'.
Khouloud.
2018-06-29 3:22 AM
Thanks - the manuals are so large that sometimes you have to know where to look.
2018-08-03 1:49 AM
The data I read is TS_CAL1:12309, TS_CAL2:15501. Temprature: 80*(HAL_ADC_GetValue(&hadc3)* 3.300f / 4096 - getTS_CAL1()) / (getTS_CAL2() - getTS_CAL1()) + 30, is it right? Is your problem solved? Can you give me the code to give me a reference?