2015-06-22 03:27 PM
I have looked and looked and cannot find what HAL stands for regarding
the HRTIM. Does anybody know what (or if) these letters mean ? Thanks, boB Everett, WA2015-06-22 04:53 PM
Hardware Abstraction Layer
2015-06-22 07:26 PM
2015-06-22 08:09 PM
STM32CubeF2 is fully compatible with STM32CubeMX code generator that allows generating initialization code. The package includes a low level hardware abstraction layer (HAL) that covers the microcontroller hardware, together with an extensive set of examples running on STMicroelectronics boards. The HAL is available in open-source BSD license for user convenience.
''