STM32F030 TIM1 trigger ADC1 (no HAL)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-06-23 1:09 AM
I am using a STM32F030-µC to control a brushless DC-Motor and i want to trigger the ADC with the TIM1. Channel 4 of the TIM1 (CC4) is programmed to look after a compare-event and the ADC should use this event to start the conversion (TRG1: TRG_CC4). Actually i have the problem that the ADC doesnt start any conversion. I read a lot of discussions but almost all developers are using the HAL-Library. However at the current state of development i dont want to use any HALs, so i masked the registers with defines from the device header. In some posts, there was the chronological order a problem. I compared the instructions of the HAL-Library with my code and adapted it. The problem is the same..
Below are the Code, especially the Init-FunctionsCan anybody help me?
Best regardsint main (void)
{
// System
SetSystemClock();
SysTickTimer_Init();
// Peripherie
GPIO_Init();
TIM1_Init();
ADC_Init();
// Start Peripherie
TIM1_SetCOM();
while (1)
{
}
}// END
void TIM1_Init (void)
{
// Timer1 clock
TIM1_ClockEnable();
// Clock Prescal-Counter: CLK_CNT = 48/2 = 24 MHz
TIM1->PSC = 0x0001;
// PWM - Frequency : 10kHz
TIM1->ARR = 2399;
// Duty-Cycle
TIM1->CCR1 = 1199; // DutyCycle 50%
TIM1->CCR2 = 1199; // -- '' --
TIM1->CCR3 = 1199; // -- '' --
TIM1->CCR4 = (TIM1->ARR)/2; //AD-Trigger
// Configuration
TIM1->CR1 &=~ TIM_CR1_DIR; // upcounting mdoe
TIM1->CR1 &=~ TIM_CR1_CMS; // Edge-aligned mode
TIM1->CR1 &=~ TIM_CR1_CKD;
TIM1->CR1 &=~ TIM_CR1_OPM;
TIM1->CR1 &=~ TIM_CR1_URS;
TIM1->CR1 &=~ TIM_CR1_UDIS; // Update enabled
TIM1->CR2 &=~ TIM_CR2_OIS1;
TIM1->CR2 &=~ TIM_CR2_OIS1N;
TIM1->CR2 &=~ TIM_CR2_OIS2;
TIM1->CR2 &=~ TIM_CR2_OIS2N;
TIM1->CR2 &=~ TIM_CR2_OIS3;
TIM1->CR2 &=~ TIM_CR2_OIS3N;
TIM1->CR2 &=~ TIM_CR2_OIS4;
TIM1->CR2 &=~ TIM_CR2_CCUS;
TIM1->CR2 |= TIM_CR2_CCPC;
TIM1->CCMR1 |= TIM_CCMR1_OC1PE; // OC1 preload enable
TIM1->CCMR1 |= TIM_CCMR1_OC1M_1 // PWM-Mode 1 (Left-aligned)
| TIM_CCMR1_OC1M_2; // --- '' ----
TIM1->CCMR1 |= TIM_CCMR1_OC2PE;
TIM1->CCMR1 |= TIM_CCMR1_OC2M_1
| TIM_CCMR1_OC2M_2;
TIM1->CCMR2 |= TIM_CCMR2_OC3PE;
TIM1->CCMR2 |= TIM_CCMR2_OC3M_1
| TIM_CCMR2_OC3M_2;
TIM1->CCMR2 &=~ TIM_CCMR2_CC4S;
TIM1->CCMR2 |= TIM_CCMR2_OC4PE;
TIM1->CCMR2 &=~ TIM_CCMR2_OC4M; // OC4 Frozen
TIM1->CCER |= TIM_CCER_CC1E; // Capture/Compare Channel 1 enable
TIM1->CCER &=~ TIM_CCER_CC1P; // Channel 1 active high
TIM1->CCER |= TIM_CCER_CC1NE;
TIM1->CCER &=~ TIM_CCER_CC1NP;
TIM1->CCER |= TIM_CCER_CC2E;
TIM1->CCER &=~ TIM_CCER_CC2P;
TIM1->CCER |= TIM_CCER_CC2NE;
TIM1->CCER &=~ TIM_CCER_CC2NP;
TIM1->CCER |= TIM_CCER_CC3E;
TIM1->CCER &=~ TIM_CCER_CC3P;
TIM1->CCER |= TIM_CCER_CC3NE;
TIM1->CCER &=~ TIM_CCER_CC3NP;
TIM1->CCER |= TIM_CCER_CC4E;
TIM1->CCER &=~ TIM_CCER_CC4P;
TIM1->BDTR |= TIM_BDTR_OSSR;
TIM1->BDTR &=~ TIM_BDTR_OSSI;
TIM1->BDTR &=~ TIM_BDTR_DTG;
TIM1->BDTR |= TIM_BDTR_DTG_4
| TIM_BDTR_DTG_5;
// Start TIM1
TIM1_Start();
// Master Output enable
TIM1->BDTR |= TIM_BDTR_MOE; // Master Output enable
}// END
void ADC_Init(void)
{
// ADC Clock Mode
ADC1->CFGR2 &=~ ADC_CFGR2_CKMODE; // ADCCLK Asynchronous Clock= 14MHz
ADC_ClockEnable();
ADC1->IER |= ADC_IER_EOCIE;
ADC1->CFGR1 &=~ ADC_CFGR1_DISCEN;
ADC1->CFGR1 &=~ ADC_CFGR1_AUTOFF;
ADC1->CFGR1 &=~ ADC_CFGR1_WAIT;
ADC1->CFGR1 &=~ ADC_CFGR1_CONT; // Single conversion mode
ADC1->CFGR1 |= ADC_CFGR1_OVRMOD;
ADC1->CFGR1 &=~ ADC_CFGR1_ALIGN; // Right alignment
ADC1->CFGR1 &=~ ADC_CFGR1_RES; // 12-Bit
ADC1->CFGR1 &=~ ADC_CFGR1_SCANDIR; // Scan Ch0 -> Ch17
ADC1->CFGR1 &=~ ADC_CFGR1_DMAEN; // DMA disabled
ADC1->CFGR1 |= ADC_CFGR1_EXTEN_0; // Hardware-Trigger rising edge
ADC1->CFGR1 |= ADC_CFGR1_EXTSEL_0; // Trigge TRG1: TIM1_CC4
ADC1->SMPR &=~ ADC_SMPR_SMP; // 1.5 ADC-clock cycles sample time
ADC1->CHSELR |= ADC_CHSELR_CHSEL9;
// Interrupt
IRQ_ADC_Init();
// ADC-Calibration
ADC1->CR |= ADC_CR_ADCAL;
while ((ADC1->CR & ADC_CR_ADCAL) == ADC_CR_ADCAL)
{}
// ADC enable
ADC1->CR = ADC_CR_ADEN;
// wait for AD-Ready
while ((ADC1->ISR & ADC_ISR_ADRDY)==0)
{}
ADC_Start();
}// END