2018-05-18 5:54 AM
Good morning,
I am developing an application that uses STM32F3DISCO as board and FreeRTOS as OS. I want to keep some data in the RAM after some Software reset that I do under some conditions so I have used the notation
__attribute__((section('.my_section')))
near the variables I want to preserve. Moreover in the linker script I have added a section just after .data and before .bss
.my_section (NOLOAD):
{ . = ALIGN(4); _s_my_section = .; *(.my_section) . = ALIGN(4) ; _e_my_section = .; } > RAMNow, the application works correctly and the values are preserved but I want to understand more:
when I do a reset pressing the button I get my values stored -> OK
when I do a power on reset values are more or less random -> OK
To put a 0 in those locations again I have to upload a program without that section defined...is the SRAM reset to 0 when a new .bin is flashed? Because otherwise I cannot explain this behavior.
Sorry if the question could seem a bit naive.
Greetings,
Davide
#soft-reset #memory-sections #ld-script #linkerSolved! Go to Solution.
2018-05-18 9:22 AM
I'd probably lean toward putting this kind of data in the top of RAM, and shrinking the memory described to the linker. Or use the BKPRAM/NVRAM if available. On the F3 the 16KB of CCMRAM might be less vulnerable to use by the tools.
>>Uhm ok thanks, so how can I be sure that I'm going to reset the region I will use to store/update those data across resets?
Storage structure has a leading signature, and trailing checksum/crc, this will fail a simple integrity check across the power-up scenario.
typedef struct _FOORAMSTRUCT {
uint32_t Sig;
uint32_t Foo;
uint32_t Bar;
uint32_t Crc;
} FOORAMSTRUCT;
FOORAMSRUCT *ramstuff = (FOORAMSRUCT *)0x10000000;
if ((ramstuff->Sig == 0xCAFECAFE) && (Crc32(0xFFFFFFFF, ramstuff, sizeof(FOORAMSTRUCT)) == 0)
{
// Structure Intact
}
else
{
// Structure Corrupt - copy in new defaults and sign
}
2018-05-18 6:12 AM
The download process usually puts a loader into RAM, and that uses other areas of RAM to perform the FLASH Erase/Write operations.
If you leave persistent data in RAM you might want to consider placing that all within a structure, and then having signatures and checksums so you can verify the integrity of that data, and copy in some new defaults when there is no valid data there.
2018-05-18 8:48 AM
Uhm ok thanks, so how can I be sure that I'm going to reset the region I will use to store/update those data across resets?
2018-05-18 9:22 AM
I'd probably lean toward putting this kind of data in the top of RAM, and shrinking the memory described to the linker. Or use the BKPRAM/NVRAM if available. On the F3 the 16KB of CCMRAM might be less vulnerable to use by the tools.
>>Uhm ok thanks, so how can I be sure that I'm going to reset the region I will use to store/update those data across resets?
Storage structure has a leading signature, and trailing checksum/crc, this will fail a simple integrity check across the power-up scenario.
typedef struct _FOORAMSTRUCT {
uint32_t Sig;
uint32_t Foo;
uint32_t Bar;
uint32_t Crc;
} FOORAMSTRUCT;
FOORAMSRUCT *ramstuff = (FOORAMSRUCT *)0x10000000;
if ((ramstuff->Sig == 0xCAFECAFE) && (Crc32(0xFFFFFFFF, ramstuff, sizeof(FOORAMSTRUCT)) == 0)
{
// Structure Intact
}
else
{
// Structure Corrupt - copy in new defaults and sign
}
2018-05-18 10:10 AM
OK then the idea is:
- when i upload a new program, RAM is used to perform some movement from/to Flash and so if I get a region filled with 0 is just by chance
- solution could be using a known region in the RAM (like you said the top) and then accessing it directly: this is a kind of absolute mapping
Thank you for the suggestion of the structure and integrity check too.
Best regards, Davide
2018-05-20 3:46 PM
Depending on the tools and implementation the startup code can often zero the statics, heap and stack. The hardware operates at a much more simplistic level, where the RAM content at startup is indeterminate and inconsequential. The reset typically clearing registers and internal states, but not iterating through memory clearing it.
2018-05-22 3:28 AM
Ok thank you, I have implemented an additional mechanism to reset those variables before the first cycle begins.
Best regards,
Davide