STM32CubeExpansion_LC_Sensor_L4_V1.0.0. stock hardfault
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-05-22 4:16 AM
Posted on May 22, 2018 at 13:16
Hello,
I am trying to run project lc_sensor_metering from STM32CubeExpansion_LC_Sensor_L4_V1.0.0. I try running it with both system workbench and segger embedded studio but it always generates a hardfault in this function:
static void LC_Init_TIM6(void)
{Htim6.Instance = TIM6;
Htim6.Init.Prescaler = 0; Htim6.Init.CounterMode = TIM_COUNTERMODE_DOWN; Htim6.Init.Period = 100; HAL_TIM_Base_Init(&Htim6);if (HAL_TIM_OnePulse_Init(&Htim6, TIM_OPMODE_SINGLE) != HAL_OK)
{ /* Initialization Error */ ErrorHandler(); }/* Enable update interrupts to use them as events for sleep mode*/
TIM6->DIER |= TIM_IT_UPDATE; TIM6->SR = ~(TIM_FLAG_UPDATE);NVIC_ClearPendingIRQ(TIM6_DAC_IRQn);}
What could possibly be wrong? The project is a example from st, I haven't changed anything, why the hardfault is generated?
Thank you
#tim6 #nucleo-l476rg #lc-sensor
Labels:
- Labels:
-
STM32L4 series
-
TIM
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0